Part Number: DLPDLCR471TPEVM Other Parts Discussed in Thread: DLPC6540 , Tool/software: DLPC6540 has only Vx1 input interface, DLPDLCR471TPEVM Front-End Board uses IT6807 for HDMI connector input.
Could you give me IT6807 datasheet or China sale's telephone…
Part Number: DLPC6540 I want to backup firmware in DLP471TPEVM via USB. I am use DLP EVM GUI 3.2.0.6.
I can get EVM Information .But when I want to backup firmware, it tell me "Firmware Backup Failed. Failed to switch to flash programming mode."
Did…
Part Number: DLPC6540 Hello, do I need to configure the software to implement the Lane remapping of DLPC6540 HSSI interface? We don't find any corresponding registers on the Software Programmer's Guide. Is it auto done? The same issue is also with remapping…
Part Number: DLPC6540 Question 1: what parallel flash can be supported
Question 2: which of the following models can support? What should I do if I need to use these chips?
S29GL256P90TFCR20 MX29GL256FHT2I-90Q MX29GL128FHT2I-70G MX29GL128FLT2I-70G…
Part Number: DLPC6540 Other Parts Discussed in Thread: DLP471TP , hi Teams:
There are multi-point correction functions for 3x3 and maximum 62x32 of DLPC 6540 IC,
Please help provide ti's demonstration program
Part Number: DLPC6540 Other Parts Discussed in Thread: DLP471TP , I had a demon system with DLP6540 formatter board connected to DLP471TP DMD. We like to know how to modify the actuator driving waveform and how to update the system to config the system…
Part Number: DLPC6540 HI, I'm trying to boot up to a new DLPC6540 projector using the following workflow:
Connect to power via 24V PSU
Connect to my laptop via a USB to TTL connector ( this one)
Use pySerial to send serial commands over TTL. …
Part Number: DLPC6540 My custoemr is asking for the voltage level specification for crystal A and B to control their materials.
Could I provide the specification for PLLMA? As I think the crystal provide a reference clock for the PLLs.
Part Number: DLPC6540 Other Parts Discussed in Thread: DLPDLCR471TPEVM Hi,
We are doing a project where we are using DLPC6540 in the solution DLPDLCR471TPEVM . We want to replace the default splash images in flash memory, by adding 10 new splash images…
Part Number: DLPC6540 Hi,
DLPC6540 requires 8-lane Vx1, what will happen when if only 2-lane Vx1 is provided ?
The resolution and color depth can be compromised
If the projector is at a fixed distance from the screen, with 4K video input (8-lane…