Part Number: DLPC7540 Other Parts Discussed in Thread: DLP660TE , DLPC4422 , , , DLP4710 , DLPC4420 , DLP780TE , DLPC900 , DLP500YX , DLP670S Hi Matt
I need your help to change Duty Cycles
for 3D printing Application, Only one led is enable and it's Duty Cycles…
Part Number: DLPC7540 Other Parts Discussed in Thread: DLPC4422 The .osddesign OSD design tool for DLPC4422 does not open the OSD design file .osddesign for DLPC754X. What tool can open the OSD design file for DLPC754X? Has the DLPC754X Platform OSD Design…
Part Number: DLPC7540 Other Parts Discussed in Thread: DLP471TE , DLPC7541 Hi expert,
I am using the DLPC7541 + DLP471TE,
When I turn on the machine for the first time, I can see something in the DMD and I can see the DMD ID and other DMD information from…
Part Number: DLPC6540 Question 1: what parallel flash can be supported
Question 2: which of the following models can support? What should I do if I need to use these chips?
S29GL256P90TFCR20 MX29GL256FHT2I-90Q MX29GL128FHT2I-70G MX29GL128FLT2I-70G S29GL2…
Part Number: DLP651NE Other Parts Discussed in Thread: DLP650TEEVM , DLPC7540EVM , DLPC7540 Tool/software: Hello
We are using DLP651NE. during On operation we see suddenly one random pixel stay on while we have it off. these one or two random pixel appear…
Hello Jianyong,
The DLPC7540 can implement 4K data processing up to 60 Hz, that is correct. The DLPC7540 is a high resolution controller and has much to offer as a solution.
I would recommend you compare the Function Block Diagrams (section 7.2) of both…
Part Number: DLP472TE Other Parts Discussed in Thread: DLP471TE , DLPC7540 Tool/software: Hello,
I am using a DLPC7540 EVM with a DLP472TE DMD however I am unable to find firmware to control the DLP472TE. On Ti's website I was only able to find firmware…
Sasaoka-san,
As described in the Design guide , there are headers/connectors that allow selecting either UDIM or SDIM for the Enables. SDIM uses the NFET shunt to turn off the LEDs. SDIM is substantially faster than using UDIM and is the only practical…
Babak,
The difference is the intended use and markets for the products.
The DLP9500 works with the DLPC410 controller. This solution is for "Advanced Light Control" (ALC) applications where control of the individual binary patterns displayed…
Hi Dimitar,
This is Siddharth and I will continue this query further.
First we need to ensure that the power supply to the DLPC7540 EVM is proper, so can you please share the details of the power supply you are using (current rating and voltage level…