Check to make sure the flex cables are connected properly and that there are no physical problems with the connectors. You will need to provide video input through a front end using mode 0x0-Disp External
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLP650TEEVM , DLPC7540 , DLP650TE Hello E2E Experts,
Good day.
I am trying to let the DLP6540TEEVM present a prestored pattern when DLPC7540EVM receives a trigger signal. Then, when receiving another…
Hi! We managed to update the firmware successfully. We used another PC with the software running in advanced mode, connected to the command interface using USB connection and in the "flash program" selected "skip bootloader" option only. (the jumper was…
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLP650TEEVM , , DLP650NE , DLP651NE , DLPC7540 Hi,
I have a brand new DLPC7540EVM, and DLP650TEEVM and it never worked properly out of the box. Am I correct in assuming that the dev board will switch…
Part Number: TPS65145 Other Parts Discussed in Thread: DLPC7540EVM , DLP650TEEVM In my design I implemented the voltage Tripler configuration as per the reference design, and the 16V supply goes to 18.5V. When I make the correction to set the board as…
Hi Made4engineering,
Thank you for waiting.
The customer had been unable to connect via UART and would need some more advice.
However, without making any changes (as far as we can tell), the firmware was able to successfully upload while we tried to get…
Part Number: DLPC7540EVM Hello Team,
My customer is looking for the STL document for DLPC7540EVM Front-end Board(the picture in the attachment).
I found the STL document is for the formatter board of DLPC7540EVM in this e2e link ( https://e2e.ti.com/support…
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLPA100 , DLPC7540 Hi,
I am working on a DLPC7540 controller board for the DLP651 DMD. Do I really need a DLPA100 if I have no need for motor control? I see that the power sequencing is not even…
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLP471TEEVM , DLP4710LC , DLP471TP , DLP471TE , DLP3010LC , DLP2010LC Hello,
I want to use DLPC7540EVM together with DLP471TEEVM as spatial light modulator. Since I don't need 4K resolution, do I have…