Part Number: DLPC900 Other Parts Discussed in Thread: DLPLCRC900EVM Hi,
When the board powers up, the heartbeat LED associated with the DLPC900 chip (D6) does not flash, but the D8 and D9 are on.
I also encountered the problem that my DMD (DLP6500) is…
Part Number: DLPC900 Other Parts Discussed in Thread: DLPC4420 Hi,
I have designed a custom board with dual DLPC900 controllers. The board is working well.
What I am wondering next is if DLPC900 controllers can be swapped with DLPC4420. I have reviewed…
Part Number: DLPC900 Hello,
I am referring to the EVM of the dual DLPC900 and redesigning a driver board. I found that the I2C signal of DLPC900 is connected to the HDMI bridge (IT6535) and the EEPROM that stores the EDID. May I ask if I can use other…
Part Number: DLP9000 I have a dual dlp900 controller setup with 2560x1600 resolution. I would like to operate with 66.6666Hz frame rate so that I can have three 5msec patterns on 15msec frame boundaries giving me an effective 200Hz pattern rate.
I have…
Part Number: DLPC900 Hello,
I have a similar limitation, but mainly concerning the automation of the 3D printing cycle. We want to sync our print stage to the advancement of the images that we would like displayed. We have done this via a python code…
Part Number: DLPC900 Hello, we are using the DPLC900 EVM in a microscopy application. We connected the EVM using HDMI to a standard PC, and so far everything is working as expected in Video Mode. We are using the DMD to project targeted beams of light…
Hello Yang,
I have few questions and observations:
Are you updating the Flash image with these images? See section 3.9.1 in Dual DLPC900 EVM User guide. Just to be certain if the patterns are added to the flash successfully, you can check the flash image…
Hello Aishwarya
For the record, the problem was that a series termination resistor from one of the clock distribution chips had popped off. Once we fixed this, we were able to turn the corner and get this working correctly. We can call this issue resolved…