Hello Aishwarya
For the record, the problem was that a series termination resistor from one of the clock distribution chips had popped off. Once we fixed this, we were able to turn the corner and get this working correctly. We can call this issue resolved…
Part Number: DLPC900 I have DLP electronics circa 2015.
How do I find out what Firmware Version is in the board sets?
Has tehere been a firmware update since then?
Part Number: DLP4620S-Q1 Other Parts Discussed in Thread: DLPC900 , DLPC230-Q1 , TPS99000-Q1 Hello experts
I have a couple of questions about the DLP4620SQ1 DMD:
1. The DMD needs to be driven by the DLPC230SQ1 controller - is this device capable of receiving…
Part Number: DLPC900
Hi
Is it posible to Invert the data inputs in a Video mode as in a pattern mode?
We would like to place the DMD9000 in a 180º (new layout) and flip Image Short-Axis , the Front light is in the same location
then we do not have…
Part Number: DLP6500FLQ Other Parts Discussed in Thread: DLPC910 , DLPC900 , , DLPLCR65EVM , DLP6500FYE , DLPLCRC900EVM , DLPLCR65FLQEVM , DLPLCRC910EVM Dear all,
I have a question regarding which controller to choose for my application when using a DLP6500FLQ…
Part Number: DLPC900 Other Parts Discussed in Thread: DLPLCRC900EVM Is there a methodology for unique identification and communication to multiple DLPC900 over USB from a single Windows PC?
Part Number: DLPC900
I am using DLP6500 with the board and I noticed that the DMD flips the image along x/y axis even though I did not use the command. I am experiencing this problem in both on-the-fly and pre-stored pattern mode. I am using labview…
Part Number: DLPC900 hello
we are using a dual controller setup of the dlpc900 and would like to read the registers of the slave directly. is that possible?
Part Number: DLPC900 Dear All,
Thank you for your supprt.
In the Pattern on-the-fly mode of the DLPC900, is it possible to upload another image into free space in the internal memory of the DLPC900 while an image is being displayed?
Best regards,
Rossinag…
Part Number: DLPC900 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
" I'm working to control the micromirror through LabVIEW, in order to do so I'm creating wrappers for the HID-API.h file found in the source code, in order…