Part Number: DLPC910 Hello,
I'd like to program DLPC910 by ISE14.7. But I could not find the IS25LP128 in PROM list of ISE14.7. How can I program it? Please see the pictures in below.
Thanks!
sunny
Hi Sunny,
I just finished talking with my coworker about this. We both think that you can remove the test points DLPC _TSTPT 0 through 15, as they are all TI Internal test points. However, I do think it is useful to have the extra ground points around…
Hello again Sunny,
If the DLP9000 is driven with the DLPC910 it simply will not configure, so you will get nothing on the DMD.
I believe the same is true if you drive the DLP9000X with the DLPC900.
There are only two differences between the DLP9000 and…
Part Number: DLPC910 Hi,
Per what consideration I set the F[2:0] pins? per DLPT030 – FEBRUARY 2023 (page 4), it only states to set the pins correctly...what does it mean? how do I choose one of the eight options?
BR
ML
Part Number: DLPC910
Hi team,
My customer want to know where can they download the FPGA source files of https://www.ti.com.cn/cn/lit/ug/dlpu125/dlpu125.pdf?ts=1688459937269&ref_url=https%253A%252F%252Fwww.ti.com.cn%252Ftool%252Fcn%252FDLPLCR90XUVEVM…
Part Number: DLP6500FLQ Other Parts Discussed in Thread: DLPC910 , DLPC900 , , DLPLCR65EVM , DLP6500FYE , DLPLCRC900EVM , DLPLCR65FLQEVM , DLPLCRC910EVM Dear all,
I have a question regarding which controller to choose for my application when using a DLP6500FLQ…
Part Number: DLPC910 Other Parts Discussed in Thread: DLP9000X ,
Hello,
I'm working with DLPC910 and DLP9000x, I'm driving DLPC with Xilinx FPGA (xcku060).
I'm having problems after few hours of work, it seems that the first rows are blank (or float…
Part Number: DLPC910 Hello
I would like to ask for some clarification on the DLPC910 PROGRAM_B pin.
- Per the datasheet it is output. but on Xilinx Virtex 5 (which the DLPC910 is based) this is an input pin.
- what is the correct functionality and direction…
Part Number: DLPC910 Other Parts Discussed in Thread: DLPC410 Hello
1. Does the DLPC910 has power up and power down requirements?
2. How does the DLPC910 power up is in relation to the DLPR910. who should ramp up first?
Thank you!