Part Number: DLP9000X I think LVDS data length should be complied within 375mm as datasheet saying. However, I would like to know the background how is the MAX length decided as 375mm. Are there problems when more length is used?
Hello Hafiz,
The DLP9000X DMD that is run by the DLPC910 controller runs at higher speed (480 MHz) than the DLP9000 DMD.(400 MHz).
If you use 405 nm then you can use the DLP9000 (DLPC900 controller) or DLP9000X (DLPC910 controller)
If you plan to use…
Part Number: DLPC910 Other Parts Discussed in Thread: DLPC410 Dear All,
In our early development phase DLPC910 will be driving with 200MHz DCLKIN speed. Does this become any issue?
Thank you and best regards,
Rossinag
Part Number: DLPC900 Other Parts Discussed in Thread: DLPC410 , DLP7000 , DLP9500 , DLP650LNIR , , DLP9000 , DLPC910 , DLP9000X , DLPC4422 , DLP660TE , DLP470TE
Hello,
Could you please help-me trying to fill correctly the values on the next table?
Empty cells…
Part Number: DLPC910 Other Parts Discussed in Thread: DLPC900 , DLPC410 The connection between DLPC910 and DLPR910 is referred to TI DLPR910 datasheet. Now, the ECP2_FINISHED signal cann't go high , which means the program cann't be loaded.
The…
Other Parts Discussed in Thread: DLPC900 , DLPC910 I am trying to figure the right DMD and controller board for my application. I have two control boards DLPC900 and DLPC910 for the DMD I am interested in in the EVM kit. The problem is I do not know how…
Part Number: DLPC910 Other Parts Discussed in Thread: DLP9000X , Hi,
We are designing the schematic of DLPC910 with DLP9000x and there are some issues below.
1. The max. input differential clock rate of DLPC910 is 480MHz. We want to confirm that the maximum…
Part Number: DLP9000XUV Other Parts Discussed in Thread: DLPC910 , DLPLCR90XUVEVM , , DLPC900 , DLP9000 , DLPLCRC910EVM Tool/software: Hello E2E Experts,
Good day.
I have recently purchased a DLP9000XUV DMD hosted by a DLPLCR90XUVEVM evaluation module for…
Part Number: DLPC910 Other Parts Discussed in Thread: TIDA-00570 , Hi,
I have a tida-00570 High Speed DLP sub-system DLPC910 Main Board. How can I test if it is available? I tried to write a breathing lamp with ISE and downloaded it through jtag, but failed…
Part Number: DLP9000 Other Parts Discussed in Thread: DLPC910 , DLPC900 , DLP7000 , , DLPLCR90EVM , DLPLCRC900DEVM Tool/software: Hi,
Customer needs a full working set to test DLP 9000 which could accept the continuous image stream to display image on DLP9000…