Hello User,
Welcome to the E2E forums and we hope to assist you with your questions.
We do not have a Linux GUI only Windows version found here:
https://www.ti.com/tool/DLPLCRD-GUI
Regards,
Alex Chan
Hello Thomas,
Firstly, I would recommend them to re-program the EVM by using the DLPLCRD-GUI with latest firmware that can be found in the Firmware selector tool .
Please let us know if the EVM still cannot work properly after re-programming, then we can…
Part Number: DLPDLCR3310EVM Hi I encounter an error while trying to change the splash logo (boot logo) for the DLPDLCR3310EVM using the
GUI FOR EVALUATION MODULE (EVM)
DLPLCRD-GUI — EVM GUI Installer for 2010, 3010, 3010-G2, 4710 and 4710-G2 EVMs.…
Part Number: DLPLCRD-GUI Other Parts Discussed in Thread: DLPC3439 , DLPNIRNANOEVM Hello
We would like to install DLPLCRD-GUI of 4710-G2 EVM to an Android OS based tablet.
Is there an Android Version of the GUI available? If not, is there a way to run the…
I dont think flashing the DLPC Flash memory with external tools is reliable, because every EVK board we are using the on board MSP430 to flash the DLPC memory, please consider my point, i need to quickly trace out why am i not able to get my re-frabricated…
Hello Valentina,
It seems like the output image doesn't appear to be cropped after you updating the firmware to v7.7.1.
Now you can switch back to DLPLCRD-GUI and try to send any commands.
For image flipping. you are be able to use Write Display Image…
Hi Jack,
The Buck GP2 is enabled by default. If you are not using PWR6, you can use the Write External PAD Address (EBh), Write External PAD Data (ECh) and Enable Register (01h) for DLPA3005 to disable the Buck GP2 [bit 4: 0 for general purpose buck 2…
Part Number: DLPC3435 Hi there,
We have built a custom board for our DLP. Currently I can flash and use the firmware provided by Texas Instruments (DLP Pico Firmware Selector), but I would like to customize the image to have new splash screens and startup…
Hello Minoru,
Welcome to DLP forum and thank you for your interest in DLP technology.
Could you please provide more details about the software tool you are using. Are you using the following GUI:
https://www.ti.com/tool/DLPLCRD-GUI
What LED duty cycle…