Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Kai Nan,
Thanks for your summary. Do you have any issues operating the GUI for this device? I am referring to the one at https://www.ti.com/tool/DLPLCRD-GUI
Have you made any modifications to the system, such as upgrading firmware or modifying MSP430 code…
Part Number: DLP160CP Other Parts Discussed in Thread: DLP160AP , , DLPDLCR3010EVM-G2 , DLPLCRD-GUI
Dear DLP customers and E2E users,
We are happy to announce the introduction of the new 0.16” nHD/QnHD DMDs: DLP160CP and DLP160AP. Using our existing portfolio…
Mark,
Yes, you can update the firmware using I2C. One of the ways to do that would be using GUI - ( https://www.ti.com/tool/DLPLCRD-GUI )
Let us know if you have any additional queries.
Regards,
Mayank
Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLPLCRD-GUI Hello,
I have a problem with the DLP® LightCrafter™ Display EVM GUI Tool. Under Windows 10 installed " DLPLCRD-GUI :
EVM GUI Installer for 2010, 3010, 3010-G2, 4710…
Mark,
There may be certain commands that ignore the read/write bit. You may want to try it both ways (with and without MSB bit) to see if your results differ.
Alternatively, you can also try sending the commands above using The LightCrafter GUI and probing…
Wladimir,
At this time, it is only possible to modify the splash images for the firmware builds which are intended for (and have a device combination matching) one of the EVMs available on TI.com. These particular firmware variants are compatible with…
User,
The DLP LightCrafter GUI tool has a feature that lets you swap the splash screen on boot to a different setup. Furthermore, the MSP430 code on the LightCrafter EVM can be configured to perform various I2C actions on system boot or when detecting…
Soizic,
Let me try to answer each of your questions individually:
Q: With the graphic interface in this document : is that possible to load images and videos from our computer? In which format ? 1104.dlpu021b.pdf
A: This is the DLP LightCrafter GUI. As…
Part Number: DLPC3435 Other Parts Discussed in Thread: DLPA2005
Hello,
We have made a custom system using DLPC3435 and would like to make a custom firmware for it.
We got one using https://www.ti.com/tool/DLP-PICO-FW-SEL
It works good, but we want for…