Part Number: DLPNIRSCANEVM The power or wake button was broken off of my DLP NIRscan Nano. I'm wondering if there is a specific part number for that I can order for it to be repaired, or if i can send it somewhere to be fixed?
Hi Takashi,
I have sent you a request to connect on E2E. Please accept this so I can send you a message to continue this conversation privately.
Thanks, Trevor
Hi Nick,
Kindly try out these steps to help us understand the problem better:
1. Kindly recheck the transistor polarity, because in the image you provided earlier it seems it is connected in opposite polarity (in reverse wrt the proper direction of…
Part Number: DLPNIRSCANEVM Hi,
I get a series of data from NIR through bluetooth, some of which are as follows:
(0x) 00-EE-0E-00-00
(0x) 01-74-70-6C-00-75-0E-00-00-53-28-75-63-23-63-63-63-63-63-63
(0x) 02-63-6A-6A-76-76-75-24-28-66-23-66-23-29…
Part Number: DLPNIRSCANEVM Hi
I’m planning to use the NIRscan Nano to regularly perform scans in a portable device.
I was wondering how this device copes with its calibration?
- How ? Is there a procedure? Calibration object?
- Frequency ? Do…
Hi MiaaTn, Our DLP Spectrum Library provides functions to deserialize the incoming scan data files. To understand the usage of this library for decoding the scan data kindly see the NIRScan Nano GUI source code, which implements and uses this functionality…
Part Number: DLPNIRSCANEVM Hello, I would like to test the DLPNIRSCANEVM: DLP® NIRscan™ Evaluation Module, however I only want to use the spectrometer and not the cuvette or the light source. Is there an option to buy only the spectrometer itself, ideally…
Part Number: DLPNIRSCANEVM Other Parts Discussed in Thread: DLPNIRNANOEVM Dear Sir,
My customer has bought the DLPNIRSCANEVM, it comes equipped with Reflective module. However, thrie application is need Transmissive module. Also, the design files listed…
Part Number: DLPNIRSCANEVM HI,
I have some doubts about the decoding function dlpspec_scan_interpret(const void *pBuf, const size_t bufSize,scanResults *pResults) given by TI and hope to get help.
The partial scanning packets I obtained through bluetooth…