Other Parts Discussed in Thread: DLPR200 , DLPC200 Hi,
I have DLP light commander development kit (Model No. DLP-LC-DLP5500-10R-A) containing 0.55XGA series 450 DMD with DLPC 200 controller and DLPA 200 Analog Driver.
I have downloaded and installed DLP…
Hi Diao,
You will need to update both GUI and MCU firmware.
For DLP LightCommander(TM) control software the latest version is 1.0.92.495. For this you will have to visit LOGIC website http://www.logicpd.com/products/application-platforms/dlp-lightcommander…
Hi Sanjeev,
Thanks so much for your reply.
We are desiring to finish the system as quick as possible.Could you give us a method that we can build it up right now?
1.For Cypress USB, we are preparing to use CyConsole tool becaue we have used it in the last…
Hi Shwetadwip Chowdhury,
Welcome to DLP&MEMS forum.
It is always suggested to start with provide GUI control software and then developing customized application. You should be able to perform the action using GUI, refer to userguide for step by step…
Hi Jeon,
The "Image Transfer APIs" are explained in the __SampleApps solution which is available on the TI network. http://www.ti.com/tool/dlpr200 and DLPR200APP component project name DownloadImagesDriverC.
The Register and LUT Read/Write…
Hi Xinyu,
Now I understand the problem you are facing. The snapshot of LC GUI version is very useful in debugging the issue. Therefore we recommend everybody to put the system version information while reporting the issue.
The _SampleApps not working…
Hi Takahashi,
Further, the DLPC200 is designed for full operation without illumination module connected i.e., without LED driver connected. Having said you must understand that the LightCommander(TM) Control GUI software is not completely tested for…
Hi Tsuboi,
Welcome to DLP & MEMS forum.
First, the DLL and libraries are generated using Visual Studio 2008 version. You should be able to find how to use older version DLLs on Visual Studio 2010 environment.
Second, from this link http://focus…
I was talking to a LogicPD representative, and she said that the "chipset itself is a TI product sold through distribution and does not come with any application software. For the chipset alone, you can work with TI or a TI authorized distributor…