Hello Nikhil,
I would recommend uninstalling any drivers that are related to the DLPC350 so they will again be reinstalled by Windows. You can also reinstall the GUI ( www.ti.com/.../dlplcr4500evm) . Lastly, if you changed the firmware at all please reflash…
Hello Franz,
Are you using the self-compiled SDK or the pre-compiled SDK? Also are what operating system are you using and what firmware version of the LightCrafter 4500 are you using? You will want to make sure you have v4.0 which is available at http…
Hi Hirak,
Are you talking about the firmware "DLPR350PROM_V3.1: CURRENT VERSION -- DLPC350 Configuration and Support Firmware", version 3.1 from here ( www.ti.com/.../dlpr350) (the marked date is 14 Jun 2017).
I believe we are already using…
Part Number: DLPLCR4500EVM Hello.
I am looking for the download link of DLPLCR4500GUI.
I have already checked following url, but I can't find it.
Could you please let me know the link?
http://www.ti.com/tool/dlplcr4500evm
http://www.tij.co.jp/tool…
Robert,
We have fixed the strange behavior issue with DMD park command as seen with F/W v3.1; this will fixed in new f/w revision v4.0.2. Please look into the DLPR350 F/W page for the update. Currently the new f/w is going under testing it will be available…
Part Number: DLPLCR4500EVM
Tool/software: Linux
Hi,
Multiple articles at the TI E2E are refering to LC4500 GUI source code (a QT project) but I cannot locate the correct file (anymore) from TI pages.
Many times this is referenced as a location for GUI…
Hi Neo,
Below are the changes in v4.0 ; you can download; it from http://www.ti.com/tool/DLPR350
F/W Version 4.0.3: * Bug-Fixes: - Solved variable exposure pattern sequence frame freeze issue when running in Variable Exposure mode and setting the pattern…
Hello Mei,
It may be very difficult to see the image change without optics. I would try to see if you can see the DMD mirrors change without illumination (i.e. look at the DMD directly, send patterns, and see if the mirror responds). If you can see the…
Hi Frederic, I think the issue is that the NIRScan EVM is not compatible with the newest version of the DLPR350 FW, you need v2.0. Do you have a copy of that FW you can load onto your device? Thanks, Paul
Hi Jeff,
Welcome to the DLP Forums and thank you for your question. Sorry about these difficulties.
For your first question, did you specify in the config_projector.txt file where the DLPR350 PROM is located on your machine?
On your second question…