Part Number: DP83825I Other Parts Discussed in Thread: DP83825 Hi Expert, We are testing the 100Base-TX compliance test and two items failed as follows. May I know which register setting can improve these two items? Thank you.
Another question, as Spec…
Part Number: DP83825I Hello,
This is simple question about Bootstrap resister value, 2.49Kohm is used for RX_D0/S(PHYADD[1]), CRS_DV/S(PHYADD[0]) , RX_D1/S(MASTER/SLAVE) on EVM.
However our customer try to minimize number of resister value.
Can they take…
Part Number: DP83825I Other Parts Discussed in Thread: DP83825 I'm using the DP83825 via RMII and not using the RX_ER pin. I'm using Energy Efficient Mode through register configuration.
Should the RX_ER pin be left floating, pulled-up or pulled…
Robert,
An additional pulse is not needed as this holding that device in reset is that pulse. Once the signal is released, the device will begin reset sequence.
Sincerely,
Gerome
Part Number: DP83825I Hi,
Good Day.
The customer is working on STM32 for Ethernet Application using PHY DP83825i.
Currently, Ethernet is up with Static Mac Address from Code.
But he wants to get the unit MAC Address From DP83825I.
How does he get it…
Part Number: DP83825I Hi experts,
For this ethernet PHY device we provided a Linux driver through 3rd party website. ( https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/drivers/net/phy/dp83822.c ) Is this driver supported by Linux…
Part Number: DP83825I Hello,
My customer had cold solder joints on a board that used the DP83825I. And the cold solder joints occurred on the four corner pins of the DP83825I device.
Please let us know if there are additional guidelines to be followed…
Part Number: DP83825I Other Parts Discussed in Thread: DP83867IR , DP83825 What do i have to write in the BISCR to set the PHY in the external loopback mode?
The data sheet of the DP83825I says that the PRBS Built-in Self-Test (BIST) can be performed using…
Part Number: DP83825I Hi,
We have made the schematic as per the attached arrangement, please review the configuration with the controller, and share the feedback on the clock and crystal used .
Also suggest any reference document for the maser and slave…