Other Parts Discussed in Thread: DP83843 Hi,
I presume that DP83843 is a non ROHS part. We would like to have the temperature profile for soldering.
Thanks and Regards
Yasser
Hi Schuyler,
Thanks for your valuable suggestion.
After making the changes in the .dts file as per your reply, the eth0 interface is not showing as below:
root@am335x-evm:~# ifconfig lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6…
Other Parts Discussed in Thread: TLK105L , DP83640 , TLK106L , DP83843 , DP83630 , DP83620 , TLK111 Hi guys,
I am currently working on a project where the communication between an Avago Fast Ethernet optical module and a PHY IC is required. I had a look at…
We are having an intermittent RX issue on a new DP83848 PHY circuit design.
The circuit design is one we have done before successfully, but we changed the layout on a new design and are having intermittent RX issues. We can transmit packets perfectly…
Hi,
Would you be able to tell me how the TD- (pin 16) and TD+ (pin 17) outputs behave while the RESET_N (pin 29) or PWR_DOWN (pin 7) inputs are asserted?
Thanks,
John
Other Parts Discussed in Thread: DP83867E Hello,
I just working on my bachelor work and I'm having to design and build an converter.
On one side there is the "Gigabit Ethernet PHY" (DP83867E) from TexasInstruments to provide the RJ45-Ethernet…
Part Number: DP83848K Other Parts Discussed in Thread: TEST2 We are using the DP83848K IC & recommended Connector : Pulse J0011D21B.
Our board is working with Ethernet speed of 10Mb/s but does not work with the 100Mb/s.
Testing Process:
1) On Board…