Part Number: DP83848C Tool/software: I am working on some ancient fw code and I am finding that the power on/boot loopback code. And I am wondering how important(required?) is it to execute loopback test at every power on/boot cycle?
thanks for your…
Part Number: DP83848C Tool/software: Hi,
I’m working on a prototype which uses the DP83848C to interface to an ESP32 using RMII. At present I’m unable to configure the PHY start up with auto-negotiation enabled.
I use pins 26 and 28 to drive LEDs…
Part Number: DP83848C Other Parts Discussed in Thread: RM46L852 , HALCOGEN Tool/software: I have DP83848 connected to RM46L852 in RMII Mode. Connections are as follows :
RM46 MDIO - DP83848 MDIO
RM46 MDC - DP83848 MDC
RM46 RMII_REFCLK_50MHZ - DP83848…
Part Number: DP83848C Tool/software: Hi team,
My customer is testing DP83848C on their PCB. They found a problem: the RMII transmit timing of their MAC cannot meet the requirements of DP83848. The "TXD[1:0], TX_EN, Data setup to X1 rising time" is required…
Part Number: DP83848C Tool/software: Hi,all
I have some questions about the VTPTD_100 in the datasheet. I wonder whether it represents the peak-to-peak value of the differential signal, or the amplitude of the single-ended signal against 0V. Can someone…
Part Number: DP83848C Tool/software: Dear Sirs ,
I am working on a layout with DP83848C and I am wondering if the PFBOUT 23 can be connected with a wire under the IC with pin 18 and 37 .
I have a bit a space constraint design and if I can rout…
Part Number: DP83848C
1. In RMII mode, MCU connects to RX-DV, but not CRS-DV.
2, RBIAS install 4.7KΩ 1% resistance.
3. PFBOUT, PFBIN1, PFBIN2 Connect to DC3.3V power supply.
The above connection. The network can be connected in actual use. Long…
Part Number: DP83848Q-Q1 Other Parts Discussed in Thread: DP83848C Tool/software: Hello support team,
The datasheet of DP83848Q-Q1 states the Vendor Model is 0xA:
but the register reads 0x9.
The datasheet of DP83848C states the Vendor Model is 0xA…