Part Number: DP83849IF Other Parts Discussed in Thread: TIDA-00306 , , DP83869 Tool/software: Hello,
I'm looking for a USB2 to 100 Mbps fiber interface. The USB host should see the interface as a new ETH interface. I plan to use any standard 1x9 SC Fiber…
Part Number: DP83849IF Other Parts Discussed in Thread: MSP430F5529
Hi forum,
we have Made a media converter pcb using DP83849IFVS ,
in that ethernet is not detecting when we connect it to the PC..
as mentioned in the schematic only we have implemented…
Part Number: DP83849IF Other Parts Discussed in Thread: DP83869 Hello TI,
We are designing a device which needs ethernet connection so for interfacing with the host we need a phy IC having following requirements which they must bear:
- Datarate (Mbps…
Part Number: DP83849IF Hi,
I think there is an algorithm that sets a timeout on the MAC side during auto-negotiation, and if it doesn't go well, restarts and repeats this, but there doesn't seem to be any regulation for this time itself. What timeout…
Part Number: DP83849IF Other Parts Discussed in Thread: DP83869HM , DP83869 , DP83822I
Hi everyone,
I'm currently looking alternate ICs for DP83849IF (which is using for Ethernet to fiber optic conversion )
So, I found few of these
DP83869HM
DP83822I …
Part Number: DP83849IF Other Parts Discussed in Thread: DP83822HF Hi TI support,
I'm developing a microcontroller board that must have a 10/100Base-T communication over twisted pair and over fiber. The two media interfaces must be available on the board…
Part Number: DP83849IF Hi,
I have to develop an unidirectional Ethernet gateway (10/100 Mbps) with a physical isolation. For this, I would like to use the 2x IC DP83849IF (copper to fiber) in media convertor mode (A -> B) <- fiber -> (B -> A) and connect…
Part Number: DP83849IF https://www.ti.com/tool/TIDA-00306
Hi, Can DP83849IF support Ethercat protocols? I believe Ethernet and Ethercat uses same physical layers so, I think it supports but I wanted to be sure. Thanks,
Part Number: DP83849IF Hello,
One of my customer did touched 8KV Discharge experiment on Ethernet interface's RJ45 shell. It seems that DP83849IF is easy to failure on the test. The customer used a multimeter to measure the impedance of Ethernet differential…