Part Number: DP83867CR Tool/software:
Subject: Assistance with WOL Function Configuration on DP83867CR
Dear TI Team,
We are currently utilizing the Wake-on-LAN (WOL) functionality of the DP83867CR and aim to configure GPIO0 to output the WOL signal.…
Part Number: DP83867CR Tool/software: Hi,
Please tell me the power supply voltage value for the internal pull-up of the RESET_N pin.
Am I correct in understanding that a 9kohm pull-up resistor and VDDIO are connected inside RESET_N?
Best Regards,
Ni…
Part Number: DP83867CR Tool/software: Hi Team,
1000Base-T compliance test failed in the customer system using DP83867CR. It passes at 100Base/10Base compliance test.
- Mask Hit in Template Test Point F test - Changed the PHY output gain, but there was…
Part Number: DP83867CR Tool/software: We are using the 1G DP83867CR ethernet PHY and have a few questions.
We have a layout constraint that requires the transformer and external signal launches to be located 12-18 inches away from the microcontroller…
Part Number: DP83867CR Tool/software: DP83867 Dual-Port TSN PCIe Application Interface Card
Hi Ti Team,
Please let us know
DP83867 Dual-Port TSN PCIe Application Interface Card will work for Dual Redundant Avionics application.
Hi Tommy,
We did not have customer ask for this register before. The register maybe reversed for external customer. We need to have a good reason to reach out to design and possibly enable this register.
If possible, may I ask the following questions…
Hi Sagar,
LED polarity depends on strap mode of LED_0 / LED_1 pin:
Modes 1/2/3 = active high
Mode 4 = active low
LED_0 cannot support mode 4. LED_1 could be inverted with mode 4, however this is only recommended if the corresponding ANEG_SEL = 1 (100…
Part Number: DP83867CR Other Parts Discussed in Thread: AM6442
Tool/software:
Hi,
I am designing an AM6442 board with LPDDR4 and DP83867 as peripherals, pwered by TPS6522053 PMIC.
I as using SK-AM64x (PROC100A) as reference.
If I keep everything the same…
Hello,
Gerome Cacho said: We do not have explicit recommendation for two level connector
Could you please introduce me to a TI engineer who is knowledgeable about PHY connectors and who might have a solution to this two-stage connector issue?
Thank you…