Part Number: DP83867CR Tool/software: Hi,
Please tell me the power supply voltage value for the internal pull-up of the RESET_N pin.
Am I correct in understanding that a 9kohm pull-up resistor and VDDIO are connected inside RESET_N?
Best Regards…
Part Number: DP83867CR Tool/software: I have modified a working design where I replaced a Marvel 88E1118R PHY with the TI DP83867CRRGZ PHY.
the PYH is located on a daughetboard with an i.MX6 Quad CPU and the RJ45 connector (MagJack V890-1AX1-A1) is…
Part Number: DP83867CR Tool/software: Hi Team,
1000Base-T compliance test failed in the customer system using DP83867CR. It passes at 100Base/10Base compliance test.
- Mask Hit in Template Test Point F test - Changed the PHY output gain, but there…
Part Number: DP83867CR Hi,
We are not providing any PU and PD combo on Rx and Tx lines so RGMII transmit clock skew and receive clock skew should be in MODE 1 which is 000 but when I am reading 6F register, I am getting 0x0155.
As per register RGMII…
Part Number: DP83867CR Hello TI team,
We are using Ethernet PHY transceiver DP83867CR in our project. We want to build a 1000m ethernet connection between DP83867CR and a PC.
We got crossover connection between D3 and D4 pair in the layout. Our…
Part Number: DP83867CR
Tool/software:
Dear Technical Support Team,
I'd like you to check my waveform because it seems not to be good signal.
However the communication itself seems to be working.
I'd like to be friendship and send my document…
Part Number: DP83867CR Tool/software: Hi Team,
Customer's use of TI DP83867CR PHY, The architecture connected to the PoE switch is as follows:
MAC uses RTL8382M (integrated 8port 1G PHY) Two external RTL8218D (8 port 1G PHY)
Customers found that…
Part Number: DP83867CR Tool/software: DP83867 Dual-Port TSN PCIe Application Interface Card
Hi Ti Team,
Please let us know
DP83867 Dual-Port TSN PCIe Application Interface Card will work for Dual Redundant Avionics application.
Part Number: DP83867CR Hello team,
On the datasheet, RBIAS should be connected with 11kohm resistor.
However, on EVM for AM62, a 22uF capacitor is connected in parallel.
Do I need this capacitor?
Best Regards, Kei Kuwahara