Part Number: DP83TD510E Tool/software: Hi, TI expert
Customer inquired if there is a TI replacement for W5100(Ethernet IC).
(See Datasheet for W5100 below)
w5100_datasheet_v1.2.6.pdf
Please check if there is a replacement.
Thank you.
Part Number: DP83TD510E-EVM Other Parts Discussed in Thread: USB-2-MDIO , Tool/software: Hello, My customer has some questions about reading registers via USB-2-MDIO as follows. Q1: At DP83TD510E-EVM, which should be selected at the Extended Register…
Part Number: DP83TD510E Tool/software: Hi Team,
We are developing APL isolators that are upstream termination is APL field switches and downstream termination is APL field devices. Would like to use DP83TD510E, there are a few questions to ask, please…
Hi Pouget,
Unfortunately, these devices are designed to be able to perform with specific input clock requirements. Such an application does not meet these requirements and is not feasible. The link speed is fixed to be 10Mbps
Best,
Vivaan
Part Number: DP83TD510E-EVM Other Parts Discussed in Thread: DP83822H , DP83TD510E Tool/software: Hi support team,
I am using two DP83TD510E-EVM modules. One EVM is connected to Laptop via RJ45 and second is connected to same way with second laptop and…
Part Number: DP83TD510E-EVM Tool/software: In SPE(Single pair Ethernet) testings on CAT6 cable of 8ohms resistance per 100m ,its working up to 600m and on power cable of 1.5sq mm 10 conductor cable its working only 300m and resistance value is 2 ohms…
Part Number: DP83TD510E Tool/software: Hello,
I designed an Ethernet to Ethernet-APL media converter using the DP83TD510E and DP83822 in back-to-back RGMII mode. It works fine if I use the straps on the DP83822 to force it to 10BASE-Te half/full duplex…
Hi Carlos,
The 10BASE-T1L products are generally suitable for 2000+ meters. The 100BASE-T1 products have been tested with cable lengths up to 15 meters. The 1000BASE-T1 products are also generally intended for cable lengths of 15 meters or less but alternate…
Part Number: DP83TD510E Tool/software: Hi SPE team,
For the DP83TD510E, how is the performance impacted when operating with a twisted pair cable with 120 Ohm differential impedance? Does it impact the cable length, power consumption, tuning? Or will…
Part Number: DP83TD510E Tool/software: Hello, My customer has questions about surge and ensuring insulation. Since 10BASE-T1L is a standard considering outdoor installation, they think that it is necessary to secure some degree of surge resistance and…