Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: TDA4VH I need to use the DP83TG720S-Q1 PHY chip to implement an interrupt when link down. In my tests, I found that register[0x12].13(Link status change interrupt status) is set and the INT_N…
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: DP83TC814S-Q1 Hi Team,
Hope you are doing well!
1. Can you provide the configuration file of DP83TG720S-Q1 Ethernet PHY? 2. Can DP83TG720S/R/-TC share a PHY configuration file?
Thanks!
Part Number: DP83TG720S-Q1 I see the 720S is a single/fixed speed PHY (1Gbps) and hence there is no auto-negotiation. It will always link-up in 1Gbps mode
leads me to my question: what is the “SGMII auto negotiation” negotiating? Master / slave ?…
Part Number: DP83TG720S-Q1 Hi,
The DP83TG720S-Q1 manual did not provide a description of register 0x56A. The customer learned through the forum that this register exists, but the reading does not match the hardware status;
Can you help provide register…
Part Number: DP83TG720S-Q1 Hi team,
Here is a question one of our customers is experiencing, could you please provide some troubleshooting suggestions?
When debugging DP83TG720S-Q1, I configured the PHY to RGMII mode and completed the initialization sequence…
Part Number: DP83TG720S-Q1 Hello team,
Happy new year.
Here is a question need your support:
During VDD power-off-> re-power-on, what is the powering off threshold before next powering up?
The VDD power rails include VDDIO, VDDA3P3 and VDD1P0.
Thanks…
Part Number: DP83TG720R-Q1 Other Parts Discussed in Thread: DP83TG720S-Q1 , Hello,
Does DP83TG720R-Q1 and DP83TG720S-Q1 support the TC10 specification?
Thanks!
Part Number: DP83TG720S-Q1 Hi team,
I recommend customers to download the PHY driver code from ti.com. However, customers reported that the official website driver cannot be compiled at present. The reason is that the official website driver kernel version…
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: DP83TG720EVM-MC Hi all,
we're evaluating the DP83TG720S-Q1 PHY with the DP83TG720EVM-MC evaluation module.
When reading the internal voltage & temperature sensors, we get realistic values…
Part Number: DP83TG720S-Q1 Hi Expert,
Does DP83TG720SWRHARQ1 could meet the requirement of ISO13400?
Customer needs the physical layer requirements for DOIP diagnostics.
Thanks a lot!
Kind Regards
Imelda