Hi,
Jin KIM said: There are two DP ports on the EVK. Is there a way to confirm DP output using the Bridge IC that switches from DSI?
Is this EVK same as the J721s2 EVM from TI in which there are 2 DP ports, Display port 0 for eDP and Display Port 1 for…
Part Number: TUSB2077A TUSB2077A User's Guide "SLLU190–December 2013"
The EVM schematic is shown in "Figure 6. TUSB2077A EVM Schematics".
Q1 in this circuit diagram pulls up DP when power is turned on.
Can this Q1 be considered…
Part Number: SK-TDA4VM 1. Download ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05-Linux-x86-Install.bin and install. 2. execute sudo ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05/bin/create-sdcard.sh, create SD rd with prebuilt Image in the sdk …
Part Number: SK-TDA4VM 1. Download ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05-Linux-x86-Install.bin and install.
2. execute sudo ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05/bin/create-sdcard.sh, create SD rd with prebuilt Image in the sd…
Part Number: SN65DP159 My design uses an SN65DP159RSBR to interface with a SMARC standard SBC card. On the DP side, the following signals are passed to the CPU on the SBC.
1. DP0+/- (Pins 6,7)
2. DP1+/- (Pins4,5)
3. DP2+/- (Pins1,2)
4. DP3+/- (Pins9,10)
5.…
Part Number: HD3SS3220 Hi Team,
May I know the reason why HD3SS3220 DFP Dongle EVM schematic TX negative connect to the positive side?
Thanks and best regards,
Jamie
Hi,
I want to use the DP on EVM board.
However is I use uenv.txt as below setting, the EVM stuck and showed message "Waiting for root device PARTUUID=99283433-02..."
====================== uenv.txt ======================>
overlay_files=
…
Part Number: TDA4VM We use TDA4 EVM to establish our ADAS prototype, we need TDA4 EVM to connect to a HDMI display.
But DP0 on the TDA4 EVM can not be converted to HDMI using an active DP to HDMI cable.
Hi David,
There are no data of Page 1 registers in the datasheet. Are these registers hidden ones?
Also, there are issues below on EVM they have. Please check and let me know.
1. There are lane0/1/2 on EyeScan settings of EyeScan tool. I think that lane0…
Part Number: J721S2XSOMXEVM
Hi,
I have been trying to use NVMe SSD storage device on J721S2XSOMXEVM board. The SSD was not able to detect due to no PCIe host bridge enabled with prebuilt image in ti-processor-sdk-rtos-j721s2-evm-09_01_00_06-prebuilt…