Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DRA75P Other Parts Discussed in Thread: DRA744 Hi everybody ,
I would like to use on a DRA744 board J6+ for higher DDR speed .
questions :
- are they pin2pin compatible ? anything particular to take care ?
- I see J6+ is about 1.3 mm less…
Hi Ram,
As informed in last week call, the OOM was being kicked in when memory was still available in the lowmem and highmem area.
This was due to virtual memory min_free_kbytes set to 3% of the RAM .
We have now reverted it to default (around 5MB), with…
Part Number: DRA744 Other Parts Discussed in Thread: CLOCKTREETOOL Tool/software: TI C/C++ Compiler Hi,
Please let know how can I get the clocktreetool for dra7xx series of SOC.
The link provided in the original e2e is not working.
Thanks
Part Number: DRA744
Tool/software: Code Composer Studio
Hi,
As my issue is not resolved yet by TI. I am trying different way to profile my code for different way of optimizing.
I am using a simulator of CCS V5 in current CCSV8.
I have created a simulator…
Part Number: DRA744 Hi , i am using DRA744 , and as I configed DDR3 timing : 0x005B0084, // EMIF1_EXT_PHY_CTRL_27 , I found that , the value changed to 0x005B006B, // EMIF1_EXT_PHY_CTRL_27 .
But according to gating description : the full-cycle tap value…
Part Number: DRA744 Linux version :ti_lts_4.4
Hi,
I have some queries on hwspinlock,
As i can see below code in driver/hwspinlock/omap_hwspinlock.c
static int omap_hwspinlock_trylock(struct hwspinlock *lock) { void __iomem *lock_addr = lock->priv;…
Part Number: DRA744 A customer unintentionally cleared all the LOCK bits (LOCK_MAINT, LOCK_PORT, LOCK_INT) of the IPU CACHE_CONFIG register when enabling caching by setting the BYPASS bit in this register to '1'. Default setting of these 3 LOCK bits is…
Part Number: DRA744 HI everybody ,
related to previous post , further investigation and it looks like new SDIO std you do not need to start 3.3V and then go 1.8V .
new std accept 1.8V all the time .
now if I set 1.8V on SDIo interface I see no activity…
Part Number: DRA744 Hi everybody ,
I m in Android 4.3 and using a WIFI module attached via SDIO signals .
WIFI module can work @ 3.3 V or 1.8V SDIO IO signals , and I am on eMMC1 .
now using signals @ 3.3V everything is fine . if I use 1.8V level ( with…