Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: DRA744 Hi,
I'm trying to display a popup on one of the VID overlay layers existing in TI DRA74x J6 processor. I'm using Linux (NOT Android). The main EGL GUI application shows its rendering output on GFX layer. My popup alert window should…
Part Number: DRA744 we have enabled early late attach feature. Included below changes as part of this
Subject: [PATCH 2/4] arm: mach-omap2: Remove edma related nodes from hwmod
init sequence
When doing late attach, kernel should not reset EDMA
EDMA…
Part Number: DRA744 Hi there,
I have 4 analog cameras which are connected over TW2964 video decoder chip to the VIP 3A port of the DRA74 J6 processor. My goal is to use VIP (Video Input Port) to capture the image frames, VPE (Video Processing Engine)…
Part Number: DRA744 Other Parts Discussed in Thread: DRA746
Hi
Due to material shortage issue that we plan replace DRA746 by DRA744.
The difference between DRA744 & DRA746 only show speed grade in DM.
Are there any difference between DRA744 & DRA746…
Part Number: DRA744 Hi
We are design new test fixture for LGA module, for the MLB testing we want connect two DRA744 through MLB as below picture.
Two DRA744 as two MLB device, the clock generated by external OSC.
Does two DRA744 can communicate by MLB…
Part Number: DRA744 Tool/software: Linux In our system, DRA744 (J6) processor is connected to a SPC560B64 micro-controller over two SPI buses (GPIO7) and also some GPIO4 pins. Linux version 4.14.40 runs on the A15 cores of J6 processor. The IPU (m4) in…
Part Number: DRA74 Hi
There are some video input port questions,
1.We use vin3a & vin4b to receive BT656 format signals( clk, D[0:7], but we could only recognize H/L by GPIO,
not in video format. Is there any setting besides these pinmux of their…
Part Number: DRA744 Other Parts Discussed in Thread: DRA714 , DRA746 Hello
We use Micrel KSZ8081MNX to receive MII signal from DRA744 before, and it's working. We change component to another MPN,Micrel KSZ8081RNB, receiving RMII signal now.
It's not…
Hi Venkat, thank you very much for sharing your patch.
We verified that applying this patch LCDs and HDMI are working togheter!!
We made also a test with the warmreset: this is necessary for the synchronization timing of the LCDs (without the warmreset…
Part Number: DRA744 Other Parts Discussed in Thread: DRA793 Hi,
which packages are available for the DRA744, and also for the DRA793?
Are the parts in this family available with a different package than BGA?
For example TQFP or LQFP?
Thanks
Fred