Part Number: DRA746 SOC: DRA746, Android8.1, kernel 4.4.117
issue: When the EVM performs the USB Accessory Test item of the CTS verify test, the EVM restarts directly and the test fails.
Test procedure: Refer to Google’s test guidelines for USB Accessory…
Part Number: DRA746 Hi team,
Here's an issue from the customer may need your help:
The customer use the android 8.1. When searching for bluetooth devices in the settings interface, it get stuck. as bellows is some logs and a picture,
Line 10208: 01…
Part Number: DRA746 Hi,
I am attempting to upgrade the linux kernel to 5.10. I can see some of the patches from the supported linux build (debian9) have been applied but some changes appear to be missing. Can I get more information on which parts have…
Part Number: PROCESSOR-SDK-DRA7X Hi,
The following folders are missing from our vision SDK TDA2xx (v03.04.00) installation
<install dir>/ti_components/os_tools/linux/kernel/omap <install dir>/ti_components/os_tools/linux/kernel/cmem/ludev/ …
Part Number: DRA746 Hi,
Now that Debian 9 (Stretch) is reaching it's end of life we would like to upgrade the kernel to Debian 10 or Debian 11. Is there any support for this with the dra746? (patches or general information).
Kind regards,
Lee
Part Number: DRA746 Other Parts Discussed in Thread: DRA744 , HI everybody ,
please can I replace DRA744BJGABCRQ1 with
DRA746PPIGABZRQ1 ? are they pin2pin ?
only difference I can see is package thickness , anything else ?
for sure I ll check PMIC consumption…
Part Number: DRA746 In the test results, there are a total of 235 modules that need to be tested, 59 of which were successfully tested, and the total number of test items for more than 100 modules is 0 (Passed 0, Failed 0, Total Tests 0). We believe …
Part Number: DRA746 Hi,
I am using gst-rtsp-server with this media pipeline:
"v4l2src device=/dev/video1 io-mode=4 ! 'video/x-raw,format=(string)YUY2,width=1920,height=1080,framerate=(fraction)30/1' ! vpe num-input-buffers=8 ! queue ! ducatih264enc intra…
Hello,
We reviewed this and SGX HW Recovery is likely an effect of an application being killed. This could be triggered by a dependency (fence) timeout. Is this always reproducible?
Regards
Hemant