Part Number: DRA80M Hi Processors Team,
My customer has followed the below links in order to flash the u-boot to eMMC.
http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_U-Boot.html#partitioning-emmc-from-u-…
Part Number: DRA80M
Hi,
Could you answer the questions I marked as green below?
V2X features/requirements
TI DRA80M
Secure Storage
V2X MUST(US,EU): Up to 10000 ECC private keys (external allowed if encrypted) 1-3MB storage,
V2X MUST(JPN):U p to…
Part Number: DRA80M I am using MMC0 to interface with an eMMC @ 3.3V. I am not using MMC1.
I currently have VDDS7 being supplied by CAP_VDDA_1P8_IOLDO0 and VDDS6 being supplied by CAP_VDDA_1P8_SDIO.
(1) Should I be using the SDIO LDO when using eMMC or…
Part Number: DRA80M Dear expert
Please help to reply as follows questions for DRA804M
1. According to datasheet, DRA804M can support LPDDR4, Could you provide the reference schematic and layout for LPDDR4 32bit ?
2. Could you have any comment for LPDDR4…
Part Number: DRA80M Tool/software: Linux I'm currently working on this for building the Linux Kernel:
http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Foundational_Components_Kernel_Users_Guide.html
When I type the following command…
Part Number: DRA80M Hello.
We have a request to interface the DRA804M SGMII to an external device with a different voltage level.
The specific questions communicated are
<quote>
The external device is 3.3V buffer circuitry but using level detection…
Part Number: DRA80M HW: DRA802
1. According to datasheet, "Power Estimation SpreadSheet provided in DRA80x Power Consumption Model." Could you provide the spreadsheet?
2. Is "Suspend to RAM" feature is supported in DRA802 based on Linux SDK…
Part Number: DRA80M Received a brief set of questions from my customer regarding the AM65xx/DRA80M device.
Which registers should be accessed in order to identify the presence of PLL? For example, in section 5.4.4.10.2, after POR MCU_PLL1 is 0 Hz (correct…
Part Number: DRA80M Tool/software: Linux I've installed Ubuntu18.04 on VirtualBox on a Dell XPS13 PC. I've been trying to go through the SDK installation steps: http://software-dl.ti.com/processor-sdk-linux/esd/docs/05_03_00_07/linux/Overview_Getting_Started_Guide…