Part Number: DRA821U Other Parts Discussed in Thread: DRA821 Hi, It seems there is no security enabled variants for DRA821U. There are only "Device type = G (General purpose)". Q1) There are several security HWA. They are PKA with ECC, AES, SHA…
Part Number: DRA821U Other Parts Discussed in Thread: DRA821 , Hello,
Can you help share the response time for the DRA821? My customer wants to know if it will be fast enough to notify a board in their system in the event of a failure mode.
Thanks, Zack …
Part Number: DRA821U Hi, My customer is asking power consumption of DAR821U. Usually PET is released to TI processors, but I could not find it for this device. Thanks and regards, Koichiro Tashiro
Part Number: DRA821U Hi TI,
Our client has two cars that occasionally experience network connectivity during testing.
TI SDK version: pdk_J7200_08_00_00_37.
Hardware connection as shown in the figure: 821 is connected to TC397 through switch, and to PC…
Part Number: DRA821U Other Parts Discussed in Thread: DRA821
I am using
Ubuntu 22.04.3 LTS
CCS12.5
pdk_j7200_09_00_01_03
I am following the instructions here
https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j7200/latest/exports/docs/psdk_rtos…
Hi,
Fhanindra Mantriraju said: bam_bootup_logs1.txt
From boot log it seems like Native Linux driver for CPSW5G. Also, you have br0 bridge interface for CPSW5G. For flow control you have to set flow-control to the respective daughter ports like (eth0, eth1…
Part Number: DRA821U
How can I build the example below that is described on this page?
PDK_09_00_01-link
Example
Application Name
Description
Cores Supported
FreeRTOS Task Switch
freertos_test_task_switch
The FreeRTOS Task Switch…
Part Number: DRA821U Hello TI Engineers,
We are now performing a power on test, and use our own dm.bin(MCU1_0) by put dm.bin file in the SD card. The ethernet can't start normally sometime.
The test sequence is power on for 35s, power off for 5s…
Yes, I do not believe it is possible to build on Windows. I have switched to Ubuntu. But there are problems building there too. see this thread
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1278742/dra821u-j7200_evm-tiarmclang…