Part Number: DRV103 I have a question regarding the maximum current output that the DRV103H can handle. The datasheet states that the maximum peak current output is between 3 and 4.2A, 3.5A nominally. I I have a solenoid that requires 3.9A for 15ms and…
Part Number: DRV103 Tool/software: Hi,
If my coil can draw up to 5A but I only need 2.5A from it, can I use the DRV103 so that it limits the current to 3.5A and the have some sort of PWM duty cycle?
Thanks.
Part Number: DRV103 Other Parts Discussed in Thread: DRV81315-Q1 Dear TI experts,
Could you check the difference between specified temperature range and operating temperature range?
Best regards,
Chase
Part Number: DRV103 Tool/software: We are currently using the DRV103 (3A PowerPad version) to drive custom solenoid valves. The DRV103 work great for the current design, and we chose to use a solenoid driver for the inbuilt over-temp, short-circuit and…
Part Number: DRV103 Other Parts Discussed in Thread: DRV8906-Q1 , DRV8912-Q1 Tool/software: Hi Team,
We are using a solenoid valve with the following specifications. The DRV103 driver is compatible. What are your suggestions for implementation/integration…
Part Number: DRV103 Other Parts Discussed in Thread: DRV8904-Q1 , DRV3946-Q1 Hello,
Do you have any values for MTBF or FIT for DRV103?
If not, can you guide me as to how to get those values?
Part Number: DRV103 Other Parts Discussed in Thread: DRV110 , , DRV120 , DRV120EVM Dear expert.
I've got a solenoid valve, which has an internal resistance of around 53 Ohm, and operate at around 10-50 V DC. When powered it around 24V Dc, its reponse…
Part Number: DRV103 Other Parts Discussed in Thread: DRV8904-Q1 Tool/software: Hello, I would like to ask for the B10, MTTF or FIT value for the DRV103H, whichever is available.
I will be using this value for a product that I am doing a pre-verification…
Part Number: DRV103 hello,
I used DRV103H in my design, in layout, power PAD via's are connected to the ground, would it make any effect on functionality of the design?
first image is viewed from ground layer. purple color is GND and orange color…
Part Number: DRV103 Other Parts Discussed in Thread: ULN2003A , Tool/software: The DRV101FKTWTG3 is currently used in one of our existing designs, and the part is now obsolete. Local suppliers are quoting over £200 per unit for a last-time buy, which…