Part Number: DRV10866 Hi team,
If customer has some thermal issue with DRV10866. Do you have suggestion? Thanks
2.5V , 0.45A temp around 44.5C
3.3V, 0.63A around around 57C
I will close this for now, since I haven't heard a response back. If you want a follow-up, please feel free to create a new thread by clicking "Ask a related question" button located on top right of this page.
Part Number: DRV10866
Hi TI Team,
Thank you for your support.
10866 TI 8AI AZ6Q 10866 TI 9BI C5TD Issue: One of our customer purchased Motor driver power MOSFET DRV10866DSCR twice. 105pcs and 40pcs But all those MOSFET has issue. (I can't believe all of…
Part Number: DRV10866 Other Parts Discussed in Thread: DRV11873 , DRV10964 , MCT8316A Hi Team, we would like to confirm if this device can be used for a bi-directional motor.
Thank you.
-Mark
Part Number: DRV10866 Hi Team,
I have a question about DRV10866 transition position from open loop to closed loop.
DRV10866 monitors BEMF zero-crossing and Once motor reaches to sufficient speed to allow four consecutive successful back-emf zero-crossing…
Part Number: DRV10866 Hello,
My customer wants to be able to monitor their motor for a locked condition. Is the easiest way to do that by monitoring the FG pin and checking for a static output (basically the same way the part itself does it)? Or is there…
Part Number: DRV10866 Hi Team,
My customer is evaluating DRV10866 and found there is voltage kick back to Vin issue when PWM duty ramp down from high to low duty. It is also found during start up at 120deg operation. Is there any recommendation to this…
Part Number: DRV10866 Other Parts Discussed in Thread: , DRV10987 , DRV10983 , DRV10964 Hi,
I am trying to use this device for a small brushless motor (Faulhaber 0308...B series). When unloaded, the device works great (much better than other third party…
Part Number: DRV10866 Hello E2E, When circuit architected at fig.4(from datasheet) that which the direction of rotation of the motor CW or CCW? Is the standard input PWM frequency to the DRV10866 25-kHz? Best regards, ACGUY
Part Number: DRV10866 Other Parts Discussed in Thread: DRV10974 Dear TI Team
I am looking for a suitable motor driver to drive the following gimbal motors.
https://www.flashhobby.com/index.php?id=3519
For example, I think DRV10866 is good. If you know…