Part Number: DRV10963 Other Parts Discussed in Thread: DRV10964 Hi Team,
Our customer is using DRV10963 in his applications. He have some questions about this device. Hoping to get your help.
The output current of DRV10963 is 500mA according to the description…
Part Number: DRV10963 I have the drv10963dsnr device that I want to use to control common hard drive platter bldc motors but I am having issues to get it to do anything. The motor specs are, Rm = 5ohms, Lm = 750uH but I do not know Kt I am using the schematic…
Other Parts Discussed in Thread: DRV10963 Hi,
My customer is using DRV10963. He has questions about FG signal. Could you answer me below questions, please?
Q1:What is FG signal generated from? -> I think that FG signal is generated from BEMF(Motor Flux…
Other Parts Discussed in Thread: DRV10963EVM , DRV10963 Hi
My customer is using DRV10963EVM. He uses motor whose pole pairs is 4. He sets FGS=1.
Could you let me know how to calculate max RPM value? He has a issue. When FG frequency exceeds 500Hz, Motor…
Other Parts Discussed in Thread: DRV10963 , DRV10963EVM , DRV10866 , DRV11873 , DRV10975 , DRV10983 Hi
I was trying to run this motor with drv10963.
www.encorerc.com/tiger-motor-gb54-1-brushless-gimbal-motor
It has 3 wire and resistance between wire is 17ohm…
Other Parts Discussed in Thread: DRV10963 , DRV10866 I tried to run a BL-DC motor from MAXON P/N: 455020 using DRV10963, I applied a 4kHz PWM signal to the PWM input, I am using 3.3V as Vcc. When the power is applied the motor runs for about 1.5sec and stalls…
Other Parts Discussed in Thread: DRV10963 Hi All,
Looking for your opinion on this issue with DRV10963 and a small three phase sensorless BLDC motor.
My question is, the driver chip only has phase U,V,W pins, but the motor I have also has 4th wire COM…
Part Number: DRV10964 Other Parts Discussed in Thread: DRV10963 , Dear team,
Is there any way tuning to align the motor's phase current to improve efficiency?
In case of DRV10963, there is Control Advance Angle function but the DRV10964 is fixed type…
Other Parts Discussed in Thread: DRV10963 I am currently using a drv10963 driver to run some prototype motors. The issue I am having is that one version of the motor will not lock on after the startup sequence. It seems that the sensorless control is unable…