Part Number: DRV10974 Other Parts Discussed in Thread: MCF8316A Tool/software: Hello TI team,
I’m currently evaluating the DRV10974 for a gimbal camera application mounted on a drone, where precise control and stability are required. One of the key…
Part Number: DRV10974 Other Parts Discussed in Thread: MCT8316A , MCT8315A Tool/software: Hi
Could you help suggest a product that can replace TOSHIBA TB67B008FNG
Part Number: DRV10974 Other Parts Discussed in Thread: DLPA100 Tool/software: Hi
DRV10974RUMR customer schematic(perhaps some resistance values need to be adjusted) I used DRV10974RUMR for the first time, but the parameters may not be adjusted properly…
Part Number: DRV10974 Other Parts Discussed in Thread: DRV10983 Tool/software: Hi team,
My customer wants to use MSPM0C and DRV10974 to realize the BLDC speed tuning.
And the target speed range and accuracy should be:
2000rpm +- 20rpm.
Could this…
Part Number: DRV10974
Tool/software:
Dear TI experts,
My customer is now in mass production stage of their own product using DRV10974.
They tests PCB assembly in production line. And sometimes they found that some assemblies make the motor spin…
Part Number: DRV10974 Hello team,
I want to set current limit to 100mA or 150mA.
On the datasheet, the example values of R(CS) is listed only from 200mA limit.
Can I set the current limit to 100mA or 150mA? If so, what would be the R(CS ) value…
Part Number: DRV10974 Other Parts Discussed in Thread: MCT8315A I need 3-Phase Brushless Sinusoidal Sensor less Motor Driver IC. Which can drive BLDC motor independently without microcontroller or any other external IC.
We need IC without CAN/LIN/SPI…
Part Number: DRV10974 Dear sir or Madam,
we're using your Motor Driver DRV10974 for an Aquarium filter, which works if we don't use any grease between the rotor axis and the enclosure around the axis (in order to Keep the axis in its Position).
As…
Part Number: DRV10974 Hi,
I coming to you cause I have a question concerning DRV10974 following Tuning guide documentaiton that is specified a Recommended Application Range for DRV10974:
What are sideeffect to using this driver whit a motor which…
Part Number: DRV10974 Other Parts Discussed in Thread: DRV10987 , DRV10975 Hi,
The customer uses the DRV10974 for the hot water mat motor control.
Stop after 1 to 2 seconds of motor initial operation.(current 0.9A)
Current Limit : 115kohm(1,400mA…