Part Number: DRV10975 Tool/software: Hi,
I would like to measure the motor force constant (N/Arms) for my motor, what I did is using Beckhoff setup I measured the position and voltage for three phases. From the position I calculated the speed, and from…
Part Number: DRV10975 Other Parts Discussed in Thread: DRV11873 , , MCF8315C Tool/software: hi team,
my customer is using DRV10975 and DRV11873. they want to know the response time of these two chips when rotating from forward changes to reverse.Thanks…
Part Number: DRV10975 Tool/software: I recently purchased a DRV10975EVM and wanted to connect it via the GUI on my PC to write the settings to the EEPROM, but it requires the power supply to be higher than 22V as shown in the attached screen.
In contrast…
Part Number: DRV10975EVM Other Parts Discussed in Thread: USB2ANY , DRV10975 Dear TI,
I have the problem to getting started with the DRV10975EVM.
OS: Windows 10
After the successful installtion of the USB2ANY interface, I stuck with the right installation…
Part Number: DRV10970 Other Parts Discussed in Thread: DRV10975 , MCT8316Z Hello,
I have been using a DRV10975 to drive a motor with 0.19mH ph-ph inductance and 0.5 Ohms ph-ph resistance from a 3-cell LiPo (11.1V nominal). I have been having trouble with…
Hi Grant,
Closing this thread as it looks like the latest response has resolved your problem.
Please help mark the thread as resolved if that's the case - and if further debug support is needed, you can click "Ask a related question" to re-open the topic…
Part Number: DRV10975 Hello,
I have been having a problem with my motor driver NACKing its own address, I know the bus works because I can communicate with other peripherals, so I was wondering if anyone else has had similar problems communicating with…
Part Number: DRV10975 Hello BLDC team:
I have some questions about "No motor fault" of DRV10975,Pealse help me to confirm.
When I config the "no motor fault" enable ,the motor will startup fail at sometimes(the motor in the hot condition…