Part Number: DRV10975 Other Parts Discussed in Thread: DRV10987 , Hi:
I can used the DRV10975EVB to control the motor speed by IIC .But it do not work in my appylication.
Following is my soft initialization:
1. 0X03 write 0X40 (enable EEPROM config)
…
Part Number: DRV10975 Hi,
If I have system with input voltage (VCC) is 12V, if the VCC voltage is cut, will the AVS function still work? When does the IC cut off this functionality?
On the programming, how does the different modes affects the register…
Part Number: DRV10975 I'm designing a board that will probably have an efficient regulated 5V supply, and will certainly have regulated 3.3V. Can I apply 5V (or 3.3V if it's all I have) to the VREG pin and leave SW disconnected to reduce power loss?…
Part Number: DRV10975 Other Parts Discussed in Thread: DRV10987 , Hi:
I can used the DRV10975EVB to control the motor speed by IIC .But it do not work in my appylication.
Following is my soft initialization:
1. 0X03 write 0X40 (enable EEPROM config)
…
Part Number: DRV10975 I'm looking for a zener to use for the DRV10975Z in 5V mode. Can I use a zener TVS for this? I'm unlikely to use a 6V zener elsewhere on my board. I'm much more likely to use a 5V TVS with a 6V breakdown voltage and high power…
Part Number: DRV10975 Hi team, please help me to guide DRV10975 PWM speed regulation control input to speed is set in the GUI environment debugging problems currently brushless motor running smooth, hope to know PWMIN input under what circumstances can…
Part Number: DRV10975 Hi,
I have some question on the Faultcore bits in the register. According to the datasheet, the bits can be reset when the motor restart, does it mean that the bits are reset by power cycling? May I know what are the conditions…
Part Number: DRV10975 Hello,
I would like to know what is the frequency range of DRV10975?
Also, how much load capacitance it provide over the I2C bus line?
Thanks a lot.