Part Number: DRV10983 Dear TI Support Team,
We are using the DRV10983 motor driver for our BLDC motor application.
Initially, we tested our motor using the DRV10983 EVM development board . The motor runs smoothly and continuously at the required speed…
Part Number: DRV10983 Other Parts Discussed in Thread: MCF8316D , MCF8315D , MOTORSTUDIO I am using the DRV10983 GUI to run a BLDC motor. Initially, everything worked normally. However, after writing the default parameters to the DRV10983 once, I started…
Part Number: DRV10983
While attempting to open the .drv file for the DRV10983 EVM , the application fails to launch and displays the following error:
"Unable to locate the LabVIEW Run-Time Engine. DRV109xx EVM requires a version 2014 (or compatible…
Part Number: DRV10983 Hello Sir/Madam,
I am unable to open the application. When I try to launch it, it prompts me to download the LabVIEW Run-Time Engine . I have already downloaded and installed the LabVIEW Run-Time Engine, but the application still…
Part Number: DRV10983 Request you to kindly provide us parameters for calculating switching loss or if you have an excel sheet for Switching loss calculation for DRV10983 kindly share us:
SRrise: Output voltage slew rate during rise (V/sec)
SRfall…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , MCF8315C-Q1 , MCF8315D , MCF8315C Hi team,
I suggest DRV10983 to replace LB11988HR for the customer.
But I checked the TI website. Find MCF8315C-Q1 spec as well.
So which one is…
Part Number: DRV10983 Tool/software: Hi
I asked a question in this link before, but unfortunately I did not get my answer. I had a experience with DRV10983 and Nanotec motor.
When I set the following values in registers, the motor spins continuously…
Part Number: DRV10983 Other Parts Discussed in Thread: MCF8315D , MOTORSTUDIO I am currently using the DRV10983 motor driver to control blower – ebmpapst RV45‑314 in our design. The motor speed is being controlled through the I²C interface.
At present…
Part Number: DRV10983 Other Parts Discussed in Thread: MCF8315D , MCF8316D Hi Team,
Posting on behalf of our customer.
I will share this E2E post to our customer so he can reply when needed.
I use a Brushless 3 Click boad which simply populates…