Part Number: DRV10983 Other Parts Discussed in Thread: MCT8316Z Tool/software: Hey
We have developed a Brushless DC (BLDC) motor with 6 poles, 18 slots, and 3 Hall sensors. The motor is driven entirely by hardware, without any microcontroller.
The…
Part Number: DRV10983 Tool/software: Hi
I would like to control a BLDC motor 50w from a 24v supply, but need to do it without a micro or software.
I need to control the speed/ torque and direction and have a static brake. will the DRV range be appropriate…
Part Number: DRV10983 Hi, Ti expert.
The customer applies DRV10983PWPR and there is a problem that the motor does not operate well during the test.
The motor seems to start initially, but there is a problem with stopping immediately. I don't know…
Part Number: DRV10983 Other Parts Discussed in Thread: , MCF8316A Hi Team,
The customer uses the DRV10983EVM control color wheel motor. The circuit architecture and DRV10983EVM GUI settings is shown as below:
The customer measured that the…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , DRV10982-Q1 ,
How do I identify the DRV10983?
Typically an I2C device can be detected purely by it's presence at an I2C address (in a closed architecture). However, some devices…
Part Number: DRV10983 Tool/software: Hi,
We are trying to switch over from using Micronel blower "Radial Blower U65ML-024KT-5" to Boreasa blower "Miniature Centrifugal Blowers C60S1-xxPR-05-Lx Series". Here are our settings for the Micronel blower:…
Part Number: DRV10983 Hello everybody,
We have the DRV10983 IC and make our PCB board tune a BLDC motor with 8 pins (U, V, W, +5, H1, H2, H3, GND). The schematic of our board is the same as the EVM DRV10983. our BLDC motor is DFA68M024037-A from Nanotec…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , TIDA-01373 , DRV10983Q1EVM , MCF8329A Tool/software: Hello. We are trying to use the DRV10983-Q1 motor driver in one of our systems. Is there any C based example code for this IC? Best…
Part Number: DRV10983 Hello,
The customer uses the chip DRV10983, which is applied at 30 revolutions per minute. The torque of the low-speed motor is small, and the motor is stuck during commissioning. Is this chip suitable for such applications?
…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: USB2ANY
Tool/software:
Hi Team,
Customer requested the configuration file using in GUI tool according to 3-phase fan parameters below, and they said that the competitor engineer(ex. MPS)…