Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 Hello experts,
Our customer encountered some problems when design DRV10983-Q1, can you help with it:
No
PN
Question describe
reply
1
DRV10983
When the LDO mode is selected…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 I am using DRV10983 for ceiling fan application. I have tuned the motor and started running only in open loop. Motor is started with align method and smoothly starts, once the fan rpm goes…
Part Number: DRV10983-Q1 Please explain all the steps involved along with the exact software versions to be installed to run DRV109xx GUI on Windows 11.
Thank you.
Part Number: DRV10983 Hi team.
What's the difference between DRV10983 and DRV10983-Q1? Can you summarize a comparison table? Can I replace DRV10983 with DRV10983-Q1 directly without changing the hardware and software?
Br,
Nison
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , , MCT8316A Hi Team,
Customer has one below square wave BLDC motor and wants to check if we can use DRV10983 sine wave method to drive, can you help to confirm it or not?
Motor's spec is…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: TIDA-01373 A little background on what has happened. I have been successfully using this driver to run a BLDC motor and control it's speed.
I was making adjustments to the configuration registers…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: MCF8316A Hi,
at the moment I'm doing some research for an application at which I need to fulfill the following points:
Controlling the output-shaft position with an accuracy approx. +/- 1…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , Hi team,
I'd like to know whether we can monitor some parameters of DRV10983 and feedback to MCU when the motor load is unconnected to IC.
I asked this because customer developed a…
Hi John,
First question is I would like to ask what is the reason for moving to DRV10983 from MCx which is FOC based?
Second question is it DRV10983 or DRV10983Q1?
Improving speed and performance with DRV10983/Q1
1. DRV10983 has Lead Time selection, this…
Part Number: DRV10983-Q1 Other Parts Discussed in Thread: DRV10983 , Hello sir, i work with the part with stm8s003f3p6. I am powering stm by 5v come from buck converter of drv10983. now problem comes when i trying turn off fan using duty down to zero the drv10983…