Part Number: DRV10983EVM Dear E2E,
I have a customized brushless dc motor that I would like to control using the DRV10983EVM. I tried to change the motor parameters and control settings after clicking on "Enable Configure" and the UI doesn't allow for…
Part Number: DRV10983EVM Other Parts Discussed in Thread: DRV10983 , USB2ANY , DRV8316 , MCT8316Z , MCT8316A , MCF8316AEVM , , MCT8316AEVM , MCF8316A Well TI you went and did it
"Notifier Timed Out Device GUI.lvlib:GUI Wait for GUI Response via Notifier…
Part Number: DRV10983EVM Hi team! This question is about software.
The customer use DRV10983EVM software( DRV109xx Software (Rev. A) )+labview2015 to test DRV10983EVM . But after installing the software, it displays as below:
What problem can cause this…
Part Number: DRV10983EVM Hi Team,
After I install DRV109xx EVM GUI, I see the notice shown in Fig.1. I install the 64bit 2022 Q3 version, 64bit 2014 SP1 version. But I still cannot run the GUI. Could you pls help? Thanks.
Fig.1:
Fig. 2:
Regards,
…
Part Number: DRV10983EVM Other Parts Discussed in Thread: DRV10983 HI,
1. Speed control of BLDC motor with DRV10983EVM using external microcontroller (Launchxl F280379d) in PWMIN mode (Duty cycle varying for speed control ).
Connection : Keeping J2 i…
Hello Vishnu,
Good day I apologize for the delay in response, my customer just got back in the office. Please see the result of their testing below:
I am answering in order:
When powering the EVM and Device with a VCC > 6.2V and VCC < 28V, is VREG…
Part Number: DRV10983EVM Other Parts Discussed in Thread: DRV10983 Hello everybody,
I'm facing a problem with DRV10983-Evalboard:
Started with Board No. 1:
Connected all needed wires and checked connections and polarity to make sure nothing goes wrong…
Part Number: DRV10983EVM Hi team
Good day
My customer need some help:
Is ok to run before , but recently DRV10983EVM and USBANY communication error
Regards
Aosker