Part Number: DRV10983EVM Can the scripting capability of DRV109xxEVM.exe evaluation software be expanded to include delays between start and stop commands to the motor? We would like to insert delays up to 10 seconds with 0.1 second resolution.
Thank…
Part Number: DRV10983EVM Hi team,
Which mode should I choose? In other word, what applications are mode 0 and mode1 suitable for? What's the benefits of mode 0 and mode 1?
Br,
Naizeng Wang
Hi TI-CSC,
It appears that the customer is referring to an old version of the DRV10983EVM users guide, the latest version of the DRV10983EVM User's Guide can be found on ti.com. We no longer provide the files referenced in the old user's guide.…
Part Number: DRV10983EVM Hello,
I am working with the DRV10983EVM and I am running my small brushless motor. It is starting and running smoothly both in open and closed loop. However, when I apply a sudden force on the rotating shaft it will stop running…
Part Number: DRV10983EVM Other Parts Discussed in Thread: USB2ANY , DRV10983
Hi Team,
Our customer is facing trouble using DRV10983EVM that they always see following error window when trying to access to the device from the GUI.
I found the following…
Part Number: DRV10983EVM I bought the DRV10983EVM, but I cannot get the GUI running with LabVIEW 2019. Now in another E2E forum I see that I need the 2014 version. But for this version I need an SSP membership. Does this mean that I cannot use the DRV10983EVM…
Part Number: DRV10983EVM Other Parts Discussed in Thread: DRV10983 Hi,
I am using the evaluation board with a small brushless DC motor but am having inconsistent issues with it. After tweaking the settings, such as motor resistance, I was able to finally…
Part Number: DRV10983EVM Other Parts Discussed in Thread: DRV10983 Hi all Would you mind if we ask DRV10983EVM? In case of low speed : Operation is OK. In case of max motor speed(450rpm) : Operation is indefinite. -> At first, should we set KT setting?…
Part Number: DRV10983EVM Other Parts Discussed in Thread: USB2ANY , DRV10983 without using usb2any explorer can i run the drv10983evm using controller??
is it possible means any example code or flow of the program or the registers.