Part Number: DRV10987 Hi Sir,
I'm working on 24V BLDC Motor driver for an air circulator Fan project which consists of 4 BLDC motors.
I have tuned all the motor drivers with the same parameters. While running the Fan, one motor is turning OFF after…
Part Number: DRV10987 Other Parts Discussed in Thread: DRV10982-Q1 Hi
We are using DRV10987 in our design. But now the same component availability is very critical and available nowhere. Kindly let me know whether we can get those parts manufactured…
Part Number: DRV10987 Hi team,
What should the overall steps be for the DRV10987 to develop software in its own circuit environment without the use of an EVM and GUI?
Step 1: It still need to determine the motor related parameters: Some of the parameters…
Part Number: DRV10987 Hi.
We want to run 2 phase brushless DC motor with DRV10987.
Is it able with DRV10987? can we disable one of phase?
and do you prefer any IC for run Brushless DC Motor at 24VDC,2A?
Part Number: DRV10987 Dear Sir/Madam,
We are getting an issue while we are driving the motor to rotate fan.
when motor/fan is rotating at low speed/starting
1)the fan is rotating back/jerk for a small time and coming forward and works normally.…
Part Number: DRV10987 Hi,
In our test setup we ran the motor above 50% dutycycle(Speed Controlling via PWM) for a certain time(at closedloop) and when we stop and restart the motor within a minute we got a fault values(8093).
May I know what will…
Part Number: MCF8316A Other Parts Discussed in Thread: DRV10987 , , , MCF8315A I have an existing design using a DRV10987. I want to upgrade to the MCF8316A, and use the same motor. I remember it was painful to figure out how to program all configuration…
Part Number: DRV10987 Hi ,
How to control speed regulation of motor . Which parameter is use to set good speed regulation .Currently motor no load speed is 424 rpm & full load speed is 352 rpm .
Part Number: DRV10987 Hi .
As the title ,my application the BLDC can't start-up success at sometimes.
I got the print information of DRV10987. Regster 0X00 Value:0004( lock2 ,abnoamal Kt),Kt value=12.38, Speed=2580 RPM(the FG frequence is 172Hz,my…