Part Number: DRV10987 Hi,
just want to get confirmation that the 10987EVM Software GUI is compatible with Windows 10.
And if so are there any extra steps needed to configure registers of the 10987 from the GUI?
thanks
Part Number: DRV10987EVM Hi, I want to operate the motor continuously using the DRV10987EVM.
The motor rotates when the command is put by speed control command. However, the current continues to increase, and motor stops by the current limit.
Then, The restart…
Part Number: DRV10987 Other Parts Discussed in Thread: USB2ANY , Hi Team,
When using the GUI of DRV10987EVM, the EVM is equipped with USB2ANY. But USB2ANY is out of stock on ti.com. Does the DRV10987 chip have to use USB2ANY when using the GUI? If the customer…
Part Number: DRV10987EVM Dear TI-er.
How do I set the correct register value?
Kt= 111.8mv/hz (by tuning guide)
My customer set the value like below.
But, It is abnormal operating status.
Can you recommand the value ?
Part Number: DRV10987EVM Other Parts Discussed in Thread: USB2ANY , DRV10983 , DRV832X Background: I'm driving an Ametek EC042B-10M0-805-SP BLDC motor from a 24V power supply.
While following the instructions in SLOU477, when I reached step 5.3 (enabling…
Part Number: DRV10987EVM Other Parts Discussed in Thread: DRV10987 ,
Tool/software: WEBENCH® Design Tools
Hi,
We are working on a 36Watt BLDC motor based on DRV10987.
Specifications of Motor
Wattage: 36Watt,
RPM: 360
Number of Poles: 16
We are facing…
Part Number: DRV10987EVM Other Parts Discussed in Thread: DRV10987 , TIDA-01373 , USB2ANY Dear, Sir.
My customer is evaluating DRV10987 using EVM & GUI.
They would like to create output file which the present configuration(resister ADRS & DATA) …
Ceyhun,
We do not have spice model for DRV10987. I would suggest to use our DRV10987EVM to learn more about the device.
https://www.ti.com/tool/DRV10987EVM
Regards,
Vishnu
Part Number: DRV10987EVM when I test my motor the three phase-to-phase resistances inductors are different. They are:
Ru-v = 3.441 ohm;Lu - v = 1535 uh
Ru-w = 3.502 ohm;Lu - w = 1735 uh
Rv-w = 2.296 ohm;Louis vuitton - w = 1296 uh
But EVM GUI can only…
Part Number: DRV10987EVM Other Parts Discussed in Thread: USB2ANY , DRV10987 Hi Cole,
my problem I have with the DRV10987EVM, which I described in the threat of Eric Chen at the 19. jan 2018 is still there not solved.
I have tried to install all Drivers…