Part Number: DRV110 Tool/software: HI all,
Im having some trouble running the simulation for a a simple DRV110 circuit. The simulation itself runs, however the results are not what i see when I test experimentally. Can somebody explain what Im doing…
Part Number: DRV3263-Q1-DESIGN-TOOL Other Parts Discussed in Thread: DRV110 Hello,
The reference design SBWM004A.TSC found on the DRV110 page doesn't appear to work properly. With no modifications to the circuit, when run in transient with 0 initial…
Part Number: DRV110 Other Parts Discussed in Thread: DRV8706-Q1 , DRV8705-Q1 Hello Ti forum,
I have to create a very strong magnetic dipole for my application, I am thinking of using anti helmholz coil to create this strong magnetic dipole. Does TI…
Part Number: DRV110 Tool/software: Hello,
I am trying to operate a contactor coil with DRV110APWR. I want the current to be around 60ma and the operating voltage should be from 80v to 250V. I have tried several combinations for Rosc and Rhold to stabilise…
Part Number: DRV110 Tool/software:
Hello,
I use a DRV110 for driving a solenoid, with a peak current of 5A and a hold current of 2A. The currents measured are correct, but I have an issue with the keep time. When the part is cold, at room temperature…
Part Number: DRV110 Tool/software: Hi all!
I'm working on a project design right now to drive a 1.5mH load at up to 13 A. I chose the DRV110 due to it being a hit/hold chip with adjustable current settings. I am using the SLIC024 calculation tool provided…
Part Number: DRV110 Tool/software: Hello team,
Is there startup sequency requirement for DRV110? Please see below, when VIN starts before EN, the relay SW is fail to operate.
The Tkeep is only 10.25mS, and the Isense is equal to Ihold. Could you…