Part Number: DRV110 Other Parts Discussed in Thread: DRV120 Hi,
I am looking for a functional substitute for DRV110 , which has available stock.
Could you please provide me any viable suggestions?
Thank you!
Regards,
Alberto
Part Number: DRV110 Hi team,
I am a FAE, who is in charge of appliance.
According to DS,"The solenoid current is ramped up fast to ensure opening of the valve or relay. After initial ramping, the solenoid current is kept at a peak value to ensure correct…
Part Number: DRV110 Hello,
My customer is wondering if they set the device up to have a 3A peak current for 4ms, and then want to switch to a 0.5A hold current, will the device make the switch even if the peak current hasn't been reached? Looking at the…
Hi Danilo/Customer,
Good to know that you have converted your application of DRV110 into acceptable performance.
Please allow me to provide additional feedback to this matter by EOW.
Thanks,
Kevin
Part Number: DRV110 Hello,
I want to design the the brakes driver circuit.
Basic Requirement is as below
Over Excitation Voltage = 24VDC
Over Excitation Power = 96W
Holding Voltage = 4VDC
Holding Power =2.7W
Over Excitation time = 150m s.
Design Paramet…
Hi Sho-san,
Like you mentioned, zener paired with solenoid, could cause the ISENSE shift, however I do not understand why this would be the case. My guess is there is an issue with SPICE model. Could you share details to your expected ISENSE value? Also…
Hi Annie,
I have a setup ready to replicate this setup. It would be most helpful if you could provide insight on what is being done with EN pin and value of VCC voltage. Does Coil+ share same source as V_IN?
Also, was this actual current measurement collected…
Part Number: DRV110 Hi, Good day. Our customer is using the DRV110PWR in their design and they have a question about the out of it. Kindly refer below. ""I am looking for an option to "bypass" the part - I mean that I will change one of the external resistor…