Part Number: DRV11873EVM Other Parts Discussed in Thread: DRV10983 , DRV10987 , DRV11873 , DRV10970 Hello,
I am using DRV11873evm to run a 12V BLDC motor. The PWM frequency I am using is 36KHZ. The FS pin setting is for 125 KHZ. The motor is running alright…
Part Number: DRV11873EVM Other Parts Discussed in Thread: DRV10975 , DRV10987 , DRV10974 , DRV11873 I am having the same problem as previously brought up. I have a 12 V BLDC motor, but when I hook it up to the driver it pulses a few times with decreasing…
Part Number: DRV11873EVM Other Parts Discussed in Thread: DRV11873 I am using DRV11873EVM to drive GB2208 motor (from http://store-en.tmotor.com/goods.php?id=447
Part Number: DRV11873EVM Other Parts Discussed in Thread: DRV11873 , , DRV10983 Hello.
Is it possible to change register settings on this DRV11873 chip with the EVM module?
I have a DRV10983 register settings that I need to copy and apply to my recently…
Part Number: DRV11873 Dear Sir,
I am using a DRV11873EVM to connect a 12 pole BLDC motor. And apply power to the H1 header, the motor starts quick smooth.
But when I adjust the R6 Potentiometer counter-clockwise to increase the speed , the motor was getting…
Part Number: DRV11873EVM I am trying to use this board to drive a brushless 3-phase dc motor. I am supplying the board with ~12V of power in and the power LED is on. The motor I am driving will pulse 3 times followed by a pause and then 3 more pulses…
I have to say, I spent the better part of the last two weeks trying to get an Atmel ATAVRMC321 development kit running without success. Tech support was no help and neither were the forums. I received the DRV11873EVM board yesterday and once I found that…
Other Parts Discussed in Thread: DRV11873EVM , DRV11873 Hi Team,
Our customer is evaluating the device using the DRV11873EVM.
They want to use the device to control the motor at 10000rpm, but the motor always stops at around 9500rpm.
What is the problem…
Other Parts Discussed in Thread: DRV11873EVM I have a 5V (850mA) BLDC motor from a hard drive connected to the DRV11873EVM board. Using the speed-adjust potentiometer (R6), I can increase the speed of the motor and I can also change its rotation (forward…
Other Parts Discussed in Thread: DRV11873 Hello,
As according to the user guide for the evaluation module, I removed the 0.0 ohm R5 resistor to allow the use of an external PWM. To test the functionality, I connected the PWM test pin from another board…