Part Number: DRV134 Tool/software: Hi,
I am checking the datasheet parameter of signal balance ratio(SBR) in positive value (i.e. 54dB). Generally, higher negative value indicates better common mode rejection. But here both min & typ values are in positive…
Part Number: DRV134 Tool/software: Hi all,
I've a single-ended to differential driver apllication replicating Fifure 29 or DRV134 datasheet; when I connect oscilloscope probe between one of the outpus and ground I get an high noise trace. Noise is lower…
Part Number: DRV134 I'm looking at the datasheet for the DRV134PA and I see a listing of 17Vrms output swing and on the graph of supply voltage vs output swing it shows roughly 19Vrms at +/- 18V. I also see that the max supply voltage is 40v or +/- 20V…
Part Number: DRV134 Hi,
I'm looking at the datasheet for this part and wondering if there is a current-limiting feature that limits the short circuit output current to 80 mA, or is there potential for it to be greater than 80 mA?
Thank you
Part Number: DRV134 Other Parts Discussed in Thread: DRV135 I am converting a design from thru hole to SMT. The thru hole design used a DRV134 in the Dip 8 package. The DRV134 in SMT is only available in SOIC-16W. I'd like to use the DRV135 SOIC-8.…
Part Number: DRV134 Hi all,
i had an issue with single supply operation, described in sloa058, chapter 1.3 AC-coupled, then i would be ensure that the DRV134 should work with single supply operation (audio application).
Thank you for your feedback.
Part Number: DRV135 Hi,
ist it possible to use multiple DRV135 on the same line to add multiple audio signals to that line?
For example, if i have 3 microphones signals (at different locations) and i would like to "mix" the signals () of all microphones…
Part Number: DRV134 I have an issue with about 10% of the DRV134 Audio-Balanced Line Drivers. On about 5 to 10% of the units tested the THD + N level is an order of 10 times higher than the published specification. Most of the parts perform as published…
Part Number: DRV134 Hi team, could you please help me to get more details of the thermal resistance for the DRV134. Into the datasheet there is only the Theta-JA Partnumber(Manuf) JB (°C/W) JC (°C/W) Tjf (°C) Tjmax (°C) DRV134UA …
Part Number: DRV134 Hello,
I am using a DRV134 in a circuit as a replacement for a SSM2142. The board is already built using 0.1uF capacitors to bypass the power supply. The DRV134 datasheet calls for 1uF capacitors.
Will the 0.1uF capacitors be a be…