Part Number: DRV135
Hellow
i`m a nalyze drv135 Using TINA ti
but I don`t understadnd Simulation result
in this condition V+ :15V, V-:-15V Vin;3V, Vo+ is 3.3V and Vo- is -3.28V
in datasheet, Gain error is noticed 0.1% at Diffrential
so, i have…
Part Number: DRV135 Hello,
is it possible to use DRV135 just as converter from single ended to differential signal, driving a high impedence imput of something else like an amplifier, and possibily decoupled with capacitors, or it is necessary to close…
Part Number: DRV135 Other Parts Discussed in Thread: DRV134 Would connecting a lower load like 75 ohms to the two output pins of the driver (instead of 600 ohms) cause any damage to the driver or voltage signal?
Part Number: DRV135 If I'm using two DRV135 audio drivers and the outputs of both drivers are tied together, will this cause damage to the one of the drivers when the other one has a stimulus applied to it? Will this cause the second drivers output to…
Part Number: DRV135 Other Parts Discussed in Thread: TLE2426 Hi ,
I would like to know some parameters of DRV135UA, see below questions:
1. The minimum single power supply of V+ (Pin 6 ) and V-(Pin 5) connect to GND?
2. Does single Power of V+ …
Part Number: DRV135 Hi,
We used DRV135 in our design and I attached the schematic. For test the thermal performance, we add the output load resistors, these are used only simulation the end user. We have 2 type of usage, one is differential output and…
Part Number: DRV135 Other Parts Discussed in Thread: OPA1637 Hi everyone,
I want to know what value is the best to operated the DRV135 . I have an audio signal generated by microcontroller where it operate with 5V. Since output microcontroller is single…
Part Number: DRV135 Hi, Good day. I hope you are doing fine. Our customer wants to use the DRV135 and they want to know if the implementation is okay. I've tried to look for a reference design unfortunately I was not able to find one. Kindly see attached…
Part Number: DRV135 Hi, The device is specified for driving a 600Ohm load, would you still get good quality audio ( do you have any data as well) driving a 300ohm load, there is some flexibility in the power supply chosen