Part Number: DRV135 If I'm using two DRV135 audio drivers and the outputs of both drivers are tied together, will this cause damage to the one of the drivers when the other one has a stimulus applied to it? Will this cause the second drivers output to…
Part Number: DRV135 Hi,
We used DRV135 in our design and I attached the schematic. For test the thermal performance, we add the output load resistors, these are used only simulation the end user. We have 2 type of usage, one is differential output and…
Part Number: DRV135 Other Parts Discussed in Thread: TLE2426 Hi ,
I would like to know some parameters of DRV135UA, see below questions:
1. The minimum single power supply of V+ (Pin 6 ) and V-(Pin 5) connect to GND?
2. Does single Power of V+ …
Part Number: DRV135 Other Parts Discussed in Thread: OPA1637 Hi everyone,
I want to know what value is the best to operated the DRV135 . I have an audio signal generated by microcontroller where it operate with 5V. Since output microcontroller is single…
Part Number: DRV135 Hi, Good day. I hope you are doing fine. Our customer wants to use the DRV135 and they want to know if the implementation is okay. I've tried to look for a reference design unfortunately I was not able to find one. Kindly see attached…
Part Number: DRV135 Hi, The device is specified for driving a 600Ohm load, would you still get good quality audio ( do you have any data as well) driving a 300ohm load, there is some flexibility in the power supply chosen
Part Number: DRV135 Other Parts Discussed in Thread: INA134 , INA137 Hi,
I am designing a balanced audio output using the DRV135, that will drive another equipment (An amplifier, exact reference unknown at this moment) via XLR connector and several…
Part Number: DRV135DRV135 makes pop noise occur.
I'm Japanese. I'm sorry my poor English.
When I supply DRV135 with a power supply, pop noise occurs.
I supply +5V and -5V to DRV135.
Delay time less than 1ms to +5V and -5V.
What is the cause…
Part Number: DRV135 Hi,
ist it possible to use multiple DRV135 on the same line to add multiple audio signals to that line?
For example, if i have 3 microphones signals (at different locations) and i would like to "mix" the signals () of all microphones…