Part Number: DRV2511-Q1 I'm trying to build a motor driver using the DRV2511. It needs to be DC coupled and I'd prefer to work out the details in TINA before creating a protoboard. Using the TI reference design "slom423.tsc" I get the following results…
Part Number: DRV2511-Q1
Hello,
We created hardware PCB as per the schematic given in EVM and connected Voice Coil Motor as LOAD. But while simulating the hardware, the LOAD and GAIN voltages are very much low than the required, like Gain voltage is…
Part Number: DRV2511-Q1 Other Parts Discussed in Thread: DRV2510-Q1 , , DRV2605L-Q1 , DRV2624 , DRV2625 , DRV2604 , DRV2605 Hi team,
My customer are selecting haptics in display project for touch vibration, which parameters should we notice? Which is…
Hi Cherry,
Cherry Zhou said: When no capacitance is added, the waveform is a normal square wave. Why does this cause the OCP to be flagged? What is the OCP tagged standard? Is it labeled as soon as 13 A is reached?
the OCP should only trip once the…
Part Number: DRV2511-Q1 I want DRV2511-Q1 to output a square wave with 50% duty.
I set the input signal as a square wave with 50% duty, but the output is a a square wave with changing duty.
What can I do to fix the output duty? How to configure the…
Hi, Yun,
Thank you for the information that you have provided.
Could you make a comparison list of the voltage level at each DRV2511-Q1 pin? You should get the same voltage level after the RC filter if all the conditions are the same than TEST1. …
Part Number: DRV2511-Q1
What is the max operating voltage for the DRV2511-Q1 logic pins FS0, FS1, FS2 and STDBY ?
In the datasheet, IN+ and IN- voltage range is -0.3V to +6.3V, and the EN pin voltage range is -0.3V to PVDD+0.3V. I also saw in another…
Part Number: DRV2511-Q1 Other Parts Discussed in Thread: DRV8876 We are developing voice coil peep valve control for our Ventilator, so please suggest me suitable driver IC for voice coil motor .
Find the attachment for Voice coil Spec and details,…
Part Number: DRV2511-Q1 Hi Team,
could you please confirm if the DRV2511 has DC output protection?
In the datasheet, it says nothing about this.
BR, Stefan
Part Number: DRV2511-Q1 Hi team,
Could you advise the minimum value of the current limit trip point of DRV2511-Q1?
No need to guarantee, but would like to know characterization data over temperature.
I choose capacitance of the output LC filter…