Part Number: DRV2511Q1EVM Tool/software: In DRV2511Q1-EVM, 60% of the waveform input to 2511 is controlled by the host computer, such as positive differential input. Why is the waveform of the output end like that on the right side of the picture? Why…
Part Number: DRV2511Q1EVM Tool/software: I am using multiple DRV2511Q1EVMs at the same time.
If I use external inputs, is there a way to enable them without connecting each board to the PC?
Part Number: DRV2511Q1EVM Tool/software: I would like to operate the DRV2511 on the EVM without using the Haptics Control Console.
Currently, the EVM seems to control the EN signal through the console software.
I'm wondering if there's a way to run…
Part Number: DRV2511Q1EVM Hi Sirs
We would like to start up DRV2511Q1EVM for haptic test.
Issue
1. No output waveform
2. "DRV on" LED light ALWAYS OFF
Process as following
1. Power external power(5V) to J5
2. Swtich S1 from 2 to 3 (Set…
Part Number: DRV2511Q1EVM Tool/software: Hello!
I'm trying to use an external PWM signal to drive the DRV2511Q1 without the on-board MSP430.
I configured the jumpers on the board according to the documentation in slou448.pdf.
I biased the (…
Part Number: DRV2511Q1EVM Hello
iam trying to connect voice coil motor VM3850RB-200 to motor driver DRV2511Q1EVM.
Please advice,
1) If the connection can be made between them ? if yes how?
2)if not, please suggest any other motor driver ic that…
Part Number: DRV2511Q1EVM I have a new DRV2511Q1EVM out of the box that is not recognized by USB.
This is what I did.
- Install and opened Haptics Control Console
- In Haptics Control Console Tools menu, selected the DRV2511
- Connected micro…
Part Number: DRV2511Q1EVM Other Parts Discussed in Thread: DRV2511-Q1 , Hello,
my customer is currently interested in the DRV2511-Q1 for one of their project and ordered DRV2511Q1EVM for some initial evaluation. However after putting the EVM into operation…
Part Number: DRV2511Q1EVM Other Parts Discussed in Thread: DRV2511-Q1 Hello experts,
When I'm reading the schematic of DRV2511Q1EVM, I find that R40 is marked with "DNP" and is not on the EVM.
I want to know the meaning of "DNP".
Accroding to the…
Part Number: DRV2511Q1EVM Hi there,
taking over this topic from Stani.
Can you please let me know the configuration of the MSP430 pins of Pins P1.4 (18) und P1.5(19) of the EVM. Are those single-ended or differential ?
Thanks,
Oz