Part Number: DRV2603 Following the datasheet, I know that value output voltage full-scale depend on value resistor of ERM.
So are there any equation to determine output voltage full-scale ?
Thanks.
Part Number: DRV2603 Other Parts Discussed in Thread: DRV2604 , DRV2604L Hello TI Team,
I am using a microcontroller that works at 1.8V.
I have a few questions reg the use of DRV2603 to drive my LRA coin vibration motor.
For my application, I want a strong…
Part Number: DRV2603 Hello,
I want to use DRV2603 to drive a vibration motor 306-114 from precision micro devices, which is not haptic feedback type . I just want to know that I can use DRV2603 to drive the motor. (Or) Is it specifically designed to drive…
Part Number: DRV2603 Other Parts Discussed in Thread: DRV2604 , DRV2605 , DRV8601 , USB2ANY
SUBJECT : DRV2603 not working properly with tested LRA HAPTIC DEVICES
The Tests have been performed with the DRV2603 EVALUATION KIT .
To compare outputs with and…
Part Number: TLC59116 Other Parts Discussed in Thread: DRV2603 , Hi. I want to drive a number of DRV2603 LRA drivers from a single command bus and I am thinking of using TLC59116 to use I2C for independantly controlling several DRV2603's. I can see that…
Part Number: DRV2603 Hi Team,
In case of LRA Mode, there is the VOUT (Differential output voltage) specification in the Electrical Characteristics, where VOUT is 2.2VRMS under VDD=3.6V and Duty Cycle=100%. And page 9, 8.4.1 LRA Mode, there is the Figure…
Part Number: DRV2603 Other Parts Discussed in Thread: DRV2625 Hi team,
my customer is designing DRV2603. According to D/S, 2.2Vrms is the best when 100%. And vibration level shows no difference under 3.3V or 5V.
Do we have a better solution which can…
Part Number: DRV2603 Hi team,
My customer wants to use our DRV2603 to drive a motor. The motor spec. is as below. Could you please evaluate if this motor is compatible to DRV2603 and which spec should be considered. Thanks.
Resistance: 8+-15% ohm
Rated…
Part Number: DRV2603 Do you have a recommended part to use with the drv2603 +-outputs for ESD protection. The outputs are connected to an external ERM motor so will potentially exposed to ESD from outside the device case. This design will have a minimum…
Part Number: DRV2603 Other Parts Discussed in Thread: DRV2624 , DRV2604 , DRV2604L Hello - We are only finding ERM motors @ 1.8VDC but we are not clear as to whether the DRV2603 driver can support this lower voltage. When we first looked at these haptics…