Part Number: DRV2603 Other Parts Discussed in Thread: DRV2625 Hello,
We are considering the DRV2603 for our application. Our actuator has a resonance frequency in the range of 250 Hz - 300 Hz.
Can the auto resonance tracking feature be used in this application…
Part Number: DRV2603 Hello,
I have an LRA application that seems to be working fine (it buzzes), but when I inspect the waveforms they're not matching the DRV2603 datasheet Figure 2. The driver seems to be skipping pulses and I was wondering if someone…
Part Number: DRV2603 Hello Team,
Well, I have a technical question about DR2603.
This IC has an output stage built in.
Can we increase its output capacity with externally attaching FET etc.
Specifically, I want to raise it to about 12 V/ 2A. If this…
Part Number: DRV2603 Other Parts Discussed in Thread: DRV2605 , DRV2625 Hi,
Out customer needs touch feedback on the products, and the needs the feature perform short period vibration (the same performance with IPHONE's touch feedback of alarm function…
Part Number: DRV2605L Other Parts Discussed in Thread: DRV2603
Hello,
I am planning to use either DRV2605L or DRV2603 in an application. I couldn't find the maximum output voltage and output current values supported by the ICs in the corresponding datasheets…
Part Number: DRV2603 Hello All! I am working on a little project similar that involves a lot of haptic feedback. So I needed a way to drive about 12+ ERM vibration motors with a few cables (i.e. NOT 12 pwm lines running to each motor). Each motor has its…
Part Number: DRV2603EVM-CT Other Parts Discussed in Thread: DRV2603 Hi. I want to make 3 levels of vibration on the device (low, middle, high), so can I control the strength of vibration with DRV2603 by changing the PWM duty cycle?
Part Number: DRV2603
Hi Team, My customer considers to use DRV2603 for ERM driver. I would like to ask the following. 1) The datasheet shows the following overcurrent protection feature but I couldn't find typical overcurrent threshold. (page 8) Could you…
Part Number: DRV2603 Hi,
I'm trying to use a DRV2603 to control a C10-000 LRA from Precision Microdrives ( www.precisionmicrodrives.com/.../c10-000-10mm-linear-resonant-actuator-3mm-type) but the vibration is "weak" and the control signals don't look…
Other Parts Discussed in Thread: DRV2603 , DRV2603EVM-CT , BQ25121 , DRV2604 , DRV2624 , DRV2604L I have a BLDC vibration motor, this one >> https://www.precisionmicrodrives.com/product/908-100-8mm-brushless-vibration-motor-3mm-type and I'm trying to drive…