Part Number: DRV2604L HI expert,
Could you please provide IBIS model for DRV2604L?
It is needed for the simulation about I2C communication in my customer side.
Thanks
Muk
Part Number: DRV2604L Other Parts Discussed in Thread: MSP430G2553 , DRV2604 Hi Team,
Customer used MSP430G2553 to drive DRV2604L, I2C cannot communicate, I2C initialization and register configuration are as follows:
/ ********************************…
Part Number: DRV2604L Hello,
we are using a DRV2604L with the LRA C08-00A.003 (Precision Microdrives).
Supply Voltage of the system is at approx. 2.8V
LRA Parameters: Rated voltage: 1.2V, Frequency: 240Hz
Unfortunately, we are not able to run an autocalibration…
Part Number: DRV2604L
HI Expert
This is similar question to following session.
My customer is using the PWM input mode for IN/TRIG pin configuration.
MODE = 3: PWM input and analog input
N_PWM_ANALOG = 0: PWM Input
The customer found the issue about…
Part Number: DRV2604 Tool/software: The customer is asking to change the i2c clock to 100KHz, but we are not able to find the timing spec for 110KHz in DRV2604L's datasheet.
May we know if we could reference IEEE's i2c timing spec when we operate…
Hi Matt,
You may be more interested in DRV2604L. DRV2605L and DRV2604L are very similar devices. The difference being that the device ending with a 5 has an integrated waveform library, but you can not alter the memory. The device ending with a 4 does…
Part Number: DRV2604L Hi Expert,
Could you please let me know I2C sink current for low drive? (Min, Typ, Max)
Also, Could you please let me know the resistance of I2C output stage(or Vol and Iol)?
Thanks
Muk
Part Number: DRV2604L Hello everyone,
I use a DRV2604L haptic driver an ERM "precision microdrive 304-103".
The configuration parameters are as follows: at. ERM_LRA - ERM b. FB_BRAKE_FACTOR [2: 0] - 2 c. LOOP_GAIN [1: 0] - 2 d. RATED_VOLTAGE [7…
Part Number: DRV2604L Hi,
We are considering using the DRV2604L for our LRA application and could not find whether or not the RAM on the driver is static, or needs to be reprogrammed after the driver has been disconnected from the source.